EAGLE User Support (English) eaglerc.erc where?
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
  • Replies 19 replies
  • Subscribers 180 subscribers
  • Views 1358 views
  • Users 0 members are here
Related

eaglerc.erc where?

autodeskguest
autodeskguest over 16 years ago

I can't find eaglerc.usr for version 5.4. I have read the update notes and

searched the specified registry key - nothing. According to the release

notes, another possible location is whatever is specified in a $HOME

variable. Well, I don't have a $HOME variable specified. Perhaps I would

specify one if I knew how but instruction seems absent.

 

What I need to do is turn off the context menu that pops up when I want to

move a group.

 

I have eaglerc.usr that was installed under version 416, and I added the

line "Option.ToggleCtrlForGroupSelectionAndContextMenu = "1"".

Naturally, version 5.4 ignores that, and the offending context menu still

inturrupts me. So, now what? I have lived with this irritation for months

and finally I can't stand it any more.

 

Maybe I should put this in the suggestions group, but why don't you just put

the eaglerc.usr file in the installation or .bin folder, and be done with

it, instead of hiding it either here or there (or NOWHERE)?

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

    Thanks to all who helped me on this. Eaglerc.usr is installed in a hidden

    folder under one of the several identities on my PC. I have made a shortcut

    to the file in a more accessable location.

     

    To eliminate the popup menu I thought I could add the following line to

    eaglerc.usr.

    "SET Option.ToggleCtrlForGroupSelectionAndContextMenu = "1""

     

    So, after spending a few hours trying to undo a so-called improvement in

    Eagle5, well, the context menu changes is still there. The fix did not work.

     

    I cannot appreciate that after grouping and right clicking the move button,

    I must then choose between a list of options, some of which don't work

    anyway. It's STUPID, but that is only my opinion.

     

    But, what about this: How am I going to mitre a group? How will I name a

    group? Split, or optimize a group?? The list goes on and on. Move is near

    the bottom of the list. GIVE ME A BREAK.

     

    Why is it even called a context menu? Most options are out of context with

    my previous mouse-clicks.

    (Where's that Xanax?)

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 16 years ago in reply to autodeskguest

    I've been using "SET Option.ToggleCtrlForGroupSelectionAndContextMenu = "1""

    for a while now.  I used to use the Control Key to prevent the Context

    Sensitive issue, but just right clicking is nicer.  My EVIL BILL VISTA OS

    does not suffer from multiple identities and the eaglerc.usr file I patched

    is in

     

    \Users\BB\AppData\Roaming\CadSoft\EAGLE.

     

    BB is my one and only username, so there's no confusion.  Eagles 5.2, 5.3

    and 5.4  all used this same location and automatically enabled the function

    after each update.  I also have "Search Hidden Folders" checked in the

    options menu so I get those results, too.

     

    You non-believing heretics will always be punished by THE EVIL BILL GOD for

    your blasphemies!  You are doomed! image

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago in reply to autodeskguest

    I've been using "SET Option.ToggleCtrlForGroupSelectionAndContextMenu = "1""

    for a while now.  I used to use the Control Key to prevent the Context

    Sensitive issue, but just right clicking is nicer.  My EVIL BILL VISTA OS

    does not suffer from multiple identities and the eaglerc.usr file I patched

    is in

     

    \Users\BB\AppData\Roaming\CadSoft\EAGLE.

     

    BB is my one and only username, so there's no confusion.  Eagles 5.2, 5.3

    and 5.4  all used this same location and automatically enabled the function

    after each update.  I also have "Search Hidden Folders" checked in the

    options menu so I get those results, too.

     

    You non-believing heretics will always be punished by THE EVIL BILL GOD for

    your blasphemies!  You are doomed! image