EAGLE User Support (English) Cannot get pad names to display in package editor
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
  • Replies 8 replies
  • Subscribers 179 subscribers
  • Views 1212 views
  • Users 0 members are here
Related

Cannot get pad names to display in package editor

autodeskguest
autodeskguest over 16 years ago

I'm having a problem with a copy of EAGLE V4.16 that I've used for the last

couple of years without problems.

 

In the last few days I've found that I can't get the pad names to display on

packages in the library editor! Both the SET PAD_NAMES ON command or the

Options -> Set->Misc->Display Pad Names menu pick check box have no effect.

If I transfer the library to another system in our office the pad names

display correctly, so I reckon it can't be the data in the library file

itself. Re-installing the EAGLE package doesn't help.

 

Is there a hidden layer I need to turn on, an .epf file or an registry entry

that's got corrupted somewhere?

 

Any help would be gratefully appreciated.

 

Malcolm Sharp

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 16 years ago

    Malcolm Sharp schrieb:

    Jörn

     

    Thanks for your reply. Unfortunately, using REDRAW command (or button) or

    any other command that causes the image to refresh still doesn't cause the

    pad names to be displayed.

     

    I don't think it is anything to do with the library files themselves as the

    pad names don't display on packages in the libraries that are part of the

    EAGLE distribution. The same libraries also work perfectly on another EAGLE

    system  we have in the office. Uninstalling and reinstalling the EAGLE

    package doesn't help either. Is there a registry entry or something that is

    retained when EAGLE is reinstalled that may have become corrupted?

     

    Regards,

     

    Malcolm

     

     

    Don't you see the pads names if you zoom further into the drawing?

    Provided "Display pad names" is active in Options/Set/Misc and the

    Pads layer or Top/Bottom layer for SMDs is displayed.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 16 years ago

    Malcolm Sharp schrieb:

    Jörn

     

    Thanks for your reply. Unfortunately, using REDRAW command (or button) or

    any other command that causes the image to refresh still doesn't cause the

    pad names to be displayed.

     

    I don't think it is anything to do with the library files themselves as the

    pad names don't display on packages in the libraries that are part of the

    EAGLE distribution. The same libraries also work perfectly on another EAGLE

    system  we have in the office. Uninstalling and reinstalling the EAGLE

    package doesn't help either. Is there a registry entry or something that is

    retained when EAGLE is reinstalled that may have become corrupted?

     

    Regards,

     

    Malcolm

     

     

    Don't you see the pads names if you zoom further into the drawing?

    Provided "Display pad names" is active in Options/Set/Misc and the

    Pads layer or Top/Bottom layer for SMDs is displayed.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm