I'm having a problem with a copy of EAGLE V4.16 that I've used for the last
couple of years without problems.
In the last few days I've found that I can't get the pad names to display on
packages in the library editor! Both the SET PAD_NAMES ON command or the
Options -> Set->Misc->Display Pad Names menu pick check box have no effect.
If I transfer the library to another system in our office the pad names
display correctly, so I reckon it can't be the data in the library file
itself. Re-installing the EAGLE package doesn't help.
Is there a hidden layer I need to turn on, an .epf file or an registry entry
that's got corrupted somewhere?
Any help would be gratefully appreciated.
Malcolm Sharp