Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Is it possible to delete part of the silkscreen of a parts footprint...?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Subscribers 189 subscribers
  • Views 2838 views
  • Users 0 members are here
  • footprint
Related

Is it possible to delete part of the silkscreen of a parts footprint...?

e14 Contributor
e14 Contributor over 12 years ago

I'm working with a design that needs to be 10cm on the x axis. My only issue is that one of the footprints has a silkscreen that measures 10.2cm. Is there any way I can cut off the last .2 cm of that footprint without editing the part? Is there a gerber editor? Some way within Eagle? Any help appreciated!

 

I've circled the area I'd like to "erase" on the right side of the board. .2 cm shaves off about to the right side of the pin labels, plenty of room. I have no need for the pin labels for that row.

image

  • Sign in to reply
  • Cancel
Parents
  • sqkybeaver
    0 sqkybeaver over 12 years ago

    you can use the smash function to separate names and values from footprint. and then individually manipulate.

     

    but you will probably have to edit the footprint from the looks of things.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to sqkybeaver

    Hmmmm ok thank you for the reply. Any idea if there is a gerber editor that could just "cut off" that area? I really want to avoid editing the package as I assume I'll have to re-route this board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to sqkybeaver

    Hmmmm ok thank you for the reply. Any idea if there is a gerber editor that could just "cut off" that area? I really want to avoid editing the package as I assume I'll have to re-route this board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to e14 Contributor

    On 9/08/2014 12:38 p.m., Nathan Coonrod wrote:

    Hmmmm ok thank you for the reply. Any idea if there is a gerber editor

    that could just "cut off" that area? I really want to avoid editing the

    package as I assume I'll have to re-route this board.

     

    .

    Really, it is easy to modify your current board using Eagle.

     

    It looks like your board outline and a few connectors holes etc are a

    package.

    Often done for Arduino shields.

     

    So make a copy of the that package in your library and then modify that

    copy.

     

    After that is done and saved, back in the board editor REPLACE the

    current part with the modified version.

     

    HTH

    Warren