Using Eagle 6.5, is there is a way to draw a line on the schematic without said line being a wire?
Thanks.
Using Eagle 6.5, is there is a way to draw a line on the schematic without said line being a wire?
Thanks.
On 8/11/2014 1:10 PM, rickford66 wrote:
Using Eagle 6.5, is there is a way to draw a line on the schematic
without said line being a wire?
Thanks.
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/123537
Oddly enough the wire command will make a line (The net command makes
wires).
Just be sure that it does not snap to any components.
So even though it has a net name, it's not going to give an error anywhere so long as it doesn't snap to any pins?
If you draw a wire on the NET layer you have created a net. You probably
don't want that.
If you want a plain old drawing wire, place a wire on a layer like SYMBOL
or INFO or create your own layer.(User defined layer)
HTH
Warren
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
On 11/08/14 22:07, rickford66 wrote:
Ah yes, there we go. I tried to move the wire from the nets layer to
another layer but it wouldn't let me. If I start that way, it works.
Yes, there are restrictions on layer swapping because it's not supposed
to be an operation that affects the fundamental design. So on the board
you can swap between copper layers but not between copper and
non-copper. Similarly the schematic editor won't let you swap a line
between "NET" and anything else because that would change the meaning.
Ah yes, there we go. I tried to move the wire from the nets layer to another layer but it wouldn't let me. If I start that way, it works. Thanks.
Ah yes, there we go. I tried to move the wire from the nets layer to another layer but it wouldn't let me. If I start that way, it works. Thanks.
On 11/08/14 22:07, rickford66 wrote:
Ah yes, there we go. I tried to move the wire from the nets layer to
another layer but it wouldn't let me. If I start that way, it works.
Yes, there are restrictions on layer swapping because it's not supposed
to be an operation that affects the fundamental design. So on the board
you can swap between copper layers but not between copper and
non-copper. Similarly the schematic editor won't let you swap a line
between "NET" and anything else because that would change the meaning.