Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Getting an error when trying to rotate a object
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 438 views
  • Users 0 members are here
Related

Getting an error when trying to rotate a object

e14 Contributor
e14 Contributor over 11 years ago

Hello,

 

This is my first time trying to use Eagle.

 

Simple project, 12 LED's on a ring.  The ring is about 2" with a 1" hole in the center.

 

I have been following the manual and was able to draw the ring on layer 20 as suggested ( I was surprised there was not "edge" or "cut" layer as in other programs).  I used the circle command to get the location and correct radius.

 

I then placed a 5mm LED from the library onto the ring.

 

I highlighted the LED and then hit properties.

 

I manipulated the X and Y to get the correct position ... no problem.

 

I then rotated the LED ......Problem ..... it let me enter the value of 0 and 180 but no angle in between.

 

When I use any other value I get the error " This Light edition of Eagle can't preform the requested action" ... next line  ...."some objects extend outside the allowed boarder area"

 

Since the ring is only 2" (50mm) and the LED is on the ring, then I would think this is not a problem.

 

Can you tell me what I am doing wrong?

 

Also, under properties, I don't see a layer listed.

 

When dropped onto the ring, will they automatically come out on the right layer ( pad on the bottom .... or top and bottom, text and symbol on top ...)?

 

Thanks so much .... Mike

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 15/08/14 00:56, Michael Csele wrote:

    Since the ring is only 2" (50mm) and the LED is on the ring, then I

    would think this is not a problem.

     

    Can you tell me what I am doing wrong?

     

    Where is the centre of the ring? The light edition requires all copper

    elements (pads, tracks) to be within a 100mm by 80mm rectangle extending

    up and right from (0 0)

     

    Also, under properties, I don't see a layer listed.

     

    When dropped onto the ring, will they automatically come out on the

    right layer ( pad on the bottom .... or top and bottom, text and symbol

    on top ...)?

     

    Components are on the top side - SMD pads on "TOP", other pads through,

    silk screen elements on top - unless "mirrored".

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to autodeskguest

    Awesome!

     

    I had made the mistake of centering the ring on 0,0 thus putting it outside the drawing area.

     

    Thanks so very much ...... Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to autodeskguest

    Awesome!

     

    I had made the mistake of centering the ring on 0,0 thus putting it outside the drawing area.

     

    Thanks so very much ...... Mike