Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Hierarchical design questions
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 189 subscribers
  • Views 933 views
  • Users 0 members are here
Related

Hierarchical design questions

cosborne2000
cosborne2000 over 11 years ago

I just upgraded to V7 and would like to convert many large schematics to a hierarchical design.

 

2 problems I'm having:

-The component name becomes very long.  The default behavior (module name:component name) seems unusable on a silk screen.

The offset method is creates huge component name values on non-trivial schematics with every module claiming values in 100 blocks.

Is there any plans on making the offset not locked to 100 increments or only checking for overlapping names with the same offset?

 

A more significant issue-

I can't find a method to cut/paste existing schematics into a hierarchical structure without the associated board locations and routing being removed for these components.

Is there a way to update a project without redoing the board layout?

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 8/21/2014 12:08 PM, cosborne2000 wrote:

    I just upgraded to V7 and would like to convert many large schematics to

    a hierarchical design.

     

    2 problems I'm having:

    -The component name becomes very long.  The default behavior (module

    name:component name) seems unusable on a silk screen.

    The offset method is creates huge component name values on non-trivial

    schematics with every module claiming values in 100 blocks.

    Is there any plans on making the offset not locked to 100 increments or

    only checking for overlapping names with the same offset?

     

    This is a work in progress and we're looking into what's the best way to

    handle this.

     

    A more significant issue-

    I can't find a method to cut/paste existing schematics into a

    hierarchical structure without the associated board locations and

    routing being removed for these components.

    Is there a way to update a project without redoing the board layout?

     

    This can be done if you put the circuits you want to convert to blocks

    as there own sheets. You can then create the modules and move the sheets

    into those modules. Sheets can be rearranged into an out of modules.

     

    hth,

    Jorge Garcia

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/124329

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cosborne2000
    0 cosborne2000 over 11 years ago in reply to autodeskguest

    Thank you for the reply.  I may be missing a step regarding transfer of a sheet into a module.

    Creating a new sheet with a circuit subset is no problem but I can't figure out the steps to convert it to a module.

     

    When I drag the sheet to the new module it still rips up the existing board.  The problem seems to be related to the net names being changed during the transition to the module.

    It would seem that the ports have to be declared simultaneously with the module creation to maintain the net.  Otherwise, Eagle rips up the board routing when the nets are modified during the transition.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • cosborne2000
    0 cosborne2000 over 11 years ago in reply to autodeskguest

    Thank you for the reply.  I may be missing a step regarding transfer of a sheet into a module.

    Creating a new sheet with a circuit subset is no problem but I can't figure out the steps to convert it to a module.

     

    When I drag the sheet to the new module it still rips up the existing board.  The problem seems to be related to the net names being changed during the transition to the module.

    It would seem that the ports have to be declared simultaneously with the module creation to maintain the net.  Otherwise, Eagle rips up the board routing when the nets are modified during the transition.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Justynb
    0 Justynb over 11 years ago in reply to autodeskguest

    Hi Jorge,

     

    Thanks for the response, however it still doesn't work for me (7.1.0 or 7.1.3 beta).

     

    This is my method, in a schematic that is already routed:

    1) Create module called TEST and place one instance.

    2) Select other components in the sheet (I've tried just a few or the entire sheet).

    3) Ctrl-right-click to pick up group.

    4) Go to module sheet TEST:1

    5) Left click to place group in module sheet.

    6) Eagle pops up with a lot of warnings of the sort: "Rename net segment 'N$1' by supply pin 'GND'?". I'm not quite sure why this happens, but whether I answer yes or no to all these popups doesn't seem to make any difference. What do these mean?

    7) All tracks in the group and the position of the components have been ripped up/reset.

     

    Is this the method you meant?

     

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Justynb

    On 11/11/2014 1:42 PM, Justyn B wrote:

    I've just tried 7.1.3 beta.

     

    I still can't find any way - I mean any way at all - of moving part of a

    schematic into a module without losing all the routing.

     

    Is there a way of doing this? I got the impression from the previous

    responses to this thread that there was meant to be.

     

     

    Currently the Hierarchy is only setup at the schematic level, there's no

    associated layout module, yet.

     

    Now when moving items between sheets you want to use the MOVE command on

    a GROUP. Even if you are only moving one part you have to do it as a

    group. In this way the layout should be preserved.

     

    hth,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Justynb
    0 Justynb over 11 years ago in reply to Justynb

    I've just tried 7.1.3 beta.

     

    I still can't find any way - I mean any way at all - of moving part of a schematic into a module without losing all the routing.

     

    Is there a way of doing this? I got the impression from the previous responses to this thread that there was meant to be.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Justynb
    0 Justynb over 11 years ago in reply to autodeskguest

    I also cannot find a way of moving already-routed parts of the board into modules.

     

    When I move the sheet into the module all the component positions reset and the tracks are lost.

     

    I've tried 7.1.0 and the beta of 7.1.1 with no luck.

     

    Am I doing something wrong or is it a bug?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to cosborne2000

    On 8/22/2014 5:16 PM, cosborne2000 wrote:

    Thank you for the reply.  I may be missing a step regarding transfer of

    a sheet into a module.

    Creating a new sheet with a circuit subset is no problem but I can't

    figure out the steps to convert it to a module.

     

    When I drag the sheet to the new module it still rips up the existing

    board.  The problem seems to be related to the net names being changed

    during the transition to the module.

    It would seem that the ports have to be declared simultaneously with the

    module creation to maintain the net.  Otherwise, Eagle rips up the board

    routing when the nets are modified during the transition.

     

    Recently,

     

    We've received reports of nets getting ripped up when net names

    change.We're looking into this I'm sure this issue is related. I'll keep

    you posted as things get resolved.

     

    Best Regards,

    Jorge Garcia