Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Is it possible to place a 'SMD' pad of a library package in an internal signal layer?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 189 subscribers
  • Views 1503 views
  • Users 0 members are here
  • pad
  • internal
  • smd
  • package
  • library
  • layer
Related

Is it possible to place a 'SMD' pad of a library package in an internal signal layer?

e14 Contributor
e14 Contributor over 12 years ago

I am designing a complex package that is going to be used repeatedly and requires the precision of a careful package layout.

 

I want to connect a schematic pin to a 'pad' on an internal signal layer of the package design. I realize that I am stretching the purpose for which a SMD pad should be used--I have no intent to surface mount anything to this pad--it will be sandwiched in an internal layer. It is simply used to tie a schematic net to a specific pad on an internal layer of the package.

 

Any ideas?

 

Thank you.

  • Sign in to reply
  • Cancel
Parents
  • kikoun
    0 kikoun over 12 years ago

    I don't thing you can do it, but you can draw copper polygon, rectangle, or wire in all layer, including internal layer.

    One solution would be to add a pad (TH type) inside that  area, maybe ?

    Guillaume.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kikoun
    0 kikoun over 12 years ago

    I don't thing you can do it, but you can draw copper polygon, rectangle, or wire in all layer, including internal layer.

    One solution would be to add a pad (TH type) inside that  area, maybe ?

    Guillaume.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to kikoun

    Guillame, thanks for your response. Let me give you some additional background on my task:

     

    I am (attempting) to design a planar transformer in Eagle. Something like this: http://upload.wikimedia.org/wikipedia/commons/5/59/Planar_core_assembly_exploded.png

     

    I want to do this as a package, as I will be reusing this part repeatedly. A transformer coil (and the routing for the core) would not be considered part of the final layout process—it is a device—it should have a symbol and package, right?

     

    My transformer is a single symbol in my schematic, with two 'pins' for each coil. If it was an external transformer, I would just connect these pins to external SMD-pads that would solder to the external device. But in this case the coils are embedded in the board and should terminate at pads to create the proper netlist and ERC from the schematic. (I realize that any undefined copper for the coils in the package will result in errors, but that easy enough to dismiss—redrawing without errors is not).


    For galvanic isolation, I do not want to tie high voltage schematic pins from a secondary coil to any SMD-pad or through-hole that is exposed to the outermost copper layers.


    From my perspective, it would be easy if I could simply place a SMD-pad on an internal layer. You already have control over pad mask, cream, and layer (bottom or top). Why not an internal layer +no cream +no mask?


    I have looked around for a while now and have found almost no one sharing how they do planar inductors in Eagle:

    Here is my exact question from a 2006 post in the EagleCentral forum (no answer): EAGLE Central Forums: eagle.support.eng » Planar magnetics with SMD-pads at inner layers

    I can find a tutorial on YouTube for Altium (but who want to spend that kind of cash when there's Eagle!): https://www.youtube.com/watch?v=qPpYDlLpjyk

     

    Best, Chris