Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Is it possible to place a 'SMD' pad of a library package in an internal signal layer?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 189 subscribers
  • Views 1502 views
  • Users 0 members are here
  • pad
  • internal
  • smd
  • package
  • library
  • layer
Related

Is it possible to place a 'SMD' pad of a library package in an internal signal layer?

e14 Contributor
e14 Contributor over 12 years ago

I am designing a complex package that is going to be used repeatedly and requires the precision of a careful package layout.

 

I want to connect a schematic pin to a 'pad' on an internal signal layer of the package design. I realize that I am stretching the purpose for which a SMD pad should be used--I have no intent to surface mount anything to this pad--it will be sandwiched in an internal layer. It is simply used to tie a schematic net to a specific pad on an internal layer of the package.

 

Any ideas?

 

Thank you.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to kikoun

    Exactly:

    Unfortunately, this feature is missing in the properties windows, so it's not easy to check our design....

    Because of the size of the transformer core all on my measurements ending up including irregular decimals, setting up the snap-to-grid with enough precision would negate the use of grid altogether. The only way to reliably do this requires me to position elements using the properties window.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kikoun
    0 kikoun over 12 years ago in reply to autodeskguest

    Hi,

    Using mark in command line is powerful when we draw or place something.

    Unfortunately, this feature is missing in the properties windows, so it's not easy to check our design....

     

    Guillaume Barrey

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to e14 Contributor

    On 08/28/2014 01:28 AM, Chris Engberg wrote:

    All of my measurements are going to have to be plus some positive value,

    making the left/right and top/bottom different values.

    Use mark and relative coordinates.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to kikoun

    Why don't you draw your coil in a new board file. In this file you only have the coil.

     

    Then, in your complete board design, you just use 'file>import>Eagle drawing' as many time as need to duplicate your coil design ?

    Then you just rename the copper trace, with the corresponding net name. In schematic, you represent the coil, by drawing a coil symbol with the net wire it self !

    It's easier than script and ulp....OK, it's only a workaround...

     

     

    I am going to give this a try. I like the fact that describing the coil with the net wire itself preserves the schematic-to-board relations.

     

    BUT I really dislike that I can't base location about the origin (as I can in the package editor) due to the license size restrictions in the board editor (requiring position on x-axis>0, y-axis>0). Frustrating. All of my measurements are going to have to be plus some positive value, making the left/right and top/bottom different values.

     

    Maybe I'll investigate Warren's suggestion to draw the coils using a ulp.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kikoun
    0 kikoun over 12 years ago in reply to autodeskguest

    Hi,

     

    Why don't you draw your coil in a new board file. In this file you only have the coil.

     

    Then, in your complete board design, you just use 'file>import>Eagle drawing' as many time as need to duplicate your coil design ?

    Then you just rename the copper trace, with the corresponding net name. In schematic, you represent the coil, by drawing a coil symbol with the net wire it self !

    It's easier than script and ulp....OK, it's only a workaround...

     

    It would be nice to have 'internal pad feature' for package design, it would be useful in your case. But not only. It could be use of internal shield, or for some component that measure the current in a PCB trace (by hall-effect)...

     

    Guillaume barrey.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago

    "Chris Engberg"  skrev i nyhetsmeldingen:

    1681421054.541408945800709.JavaMail.jive@flmspu-csapp-02.premierfarnell.com

    ...

     

    I am designing a complex package that is going to be used repeatedly and

    requires the precision of a careful package layout.

     

    I want to connect a schematic pin to a 'pad' on an internal signal layer

    of the package design. I realize that I am stretching the purpose for

    which a SMD pad should be used--I have no intent to surface mount

    anything to this pad--it will be sandwiched in an internal layer. It is

    simply used to tie a schematic net to a specific pad on an internal

    layer of the package.

     

    Why can't you just use a dummy pad with no mask at ends? You will eventually

    need to bring it out to some component after all.

    I made this little attached project for testing.

    Use the 7zip tool, free downloadable at 7zip.org to unpack.

     

    Attachments:
    test.7z.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to e14 Contributor

    On 26/08/2014 11:47 a.m., Chris Engberg wrote:

     

    .....I am (attempting) to design a planar transformer in Eagle. Something

    like this:

    http://upload.wikimedia.org/wikipedia/commons/5/59/Planar_core_assembly_exploded.png

     

    I want to do this as a package, as I will be reusing this part

    repeatedly. A transformer coil (and the routing for the core) would not

    be considered part of the final layout process—it is a device—it should

    have a symbol and package, right?

     

    My transformer is a single symbol in my schematic, with two 'pins' for

    each coil. If it was an external transformer, I would just connect these

    pins to external SMD-pads that would solder to the external device. But

    in this case the coils are embedded in the board and should terminate at

    pads to create the proper netlist and ERC from the schematic. (I realize

    that any undefined copper for the coils in the package will result in

    errors, but that easy enough to dismiss—redrawing without errors is

    not).

     

     

    For galvanic isolation, I do not want to tie high voltage schematic pins

    from a secondary coil to any SMD-pad or through-hole that is exposed to

    the outermost copper layers.

     

     

    From my perspective, it would be easy if I could simply place a SMD-pad

    on an internal layer. You already have control over pad mask, cream, and

    layer (bottom or top). Why not an internal layer +no cream +no mask?

     

     

     

     

    You cannot do it with a standard Eagle device for a number of reasons

    the biggest being there are no vias in a package, only pads which drill

    from top to bottom. Pad stacks are something asked for over the years

    but still have not arrived.

     

    I would do what you want the following way:

    You make some of what you want as a package and the rest is created on

    the board once. You then you create a script that describes the coils.

     

    There may need to be a ULP to translate the relative coords of the coils

    to the place in the future board.

     

    The package gives the part an origin that the script will reference

    Add the routing for the 'C'/'E' core holes

    Add the tPlace (silk screen print)

    Add outer SMD as needed to match with the pins of the schematic symbols

    Add anything else that can be done when making the package.

     

    Then on a new board:

    Add the package

    Draw the coils

    Add via between the layers as required

    Delete the package

    Run the ULP that gathers up the details on the coil(wires)

     

    That's it in a nutshell

    You could practice with the ulps that eagle includes

    spiral-coil.ulp

    That gives you a coil with two vias to play with.

    copy-layer-to-any-layer.ulp

    That shows you the wires before it draws them. You could copy the

    details of your layer using that.

     

    Anyway thats the drift of a technique.

     

    HTH

    Warren

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to kikoun

    Guillame, thanks for your response. Let me give you some additional background on my task:

     

    I am (attempting) to design a planar transformer in Eagle. Something like this: http://upload.wikimedia.org/wikipedia/commons/5/59/Planar_core_assembly_exploded.png

     

    I want to do this as a package, as I will be reusing this part repeatedly. A transformer coil (and the routing for the core) would not be considered part of the final layout process—it is a device—it should have a symbol and package, right?

     

    My transformer is a single symbol in my schematic, with two 'pins' for each coil. If it was an external transformer, I would just connect these pins to external SMD-pads that would solder to the external device. But in this case the coils are embedded in the board and should terminate at pads to create the proper netlist and ERC from the schematic. (I realize that any undefined copper for the coils in the package will result in errors, but that easy enough to dismiss—redrawing without errors is not).


    For galvanic isolation, I do not want to tie high voltage schematic pins from a secondary coil to any SMD-pad or through-hole that is exposed to the outermost copper layers.


    From my perspective, it would be easy if I could simply place a SMD-pad on an internal layer. You already have control over pad mask, cream, and layer (bottom or top). Why not an internal layer +no cream +no mask?


    I have looked around for a while now and have found almost no one sharing how they do planar inductors in Eagle:

    Here is my exact question from a 2006 post in the EagleCentral forum (no answer): EAGLE Central Forums: eagle.support.eng » Planar magnetics with SMD-pads at inner layers

    I can find a tutorial on YouTube for Altium (but who want to spend that kind of cash when there's Eagle!): https://www.youtube.com/watch?v=qPpYDlLpjyk

     

    Best, Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kikoun
    0 kikoun over 12 years ago

    I don't thing you can do it, but you can draw copper polygon, rectangle, or wire in all layer, including internal layer.

    One solution would be to add a pad (TH type) inside that  area, maybe ?

    Guillaume.