Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 5.4.0 started crashing, Windows SP sp3
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 189 subscribers
  • Views 1557 views
  • Users 0 members are here
Related

Eagle 5.4.0 started crashing, Windows SP sp3

blewis999
blewis999 over 17 years ago

Eagle has started terminating, I have loaded no new programs or

drivers. I tried rolling windows back to when the system was stable.

Only Eagle is crashing, none of the other programs have this problem.

Has anyone else encountered this, and if so what can be done. I tried

re-installing but same problem. Although I did install into the same

directory and just overwrote the files.

 

  • Sign in to reply
  • Cancel
Parents
  • blewis999
    blewis999 over 17 years ago

    Unfortunately, Eagle 5.4.0 just terminated again but this time there

    are no events in the system log.

     

    I am not sure what to do... I do not have any other app's terminating.

    I just upgraded from Eagle 4.16r1 and have never had that version

    crash. I used 4.16r1 up to the time I installed 5.4.0 without problem

    and did no system upgrades between the install of 5.4 and using 4.16.

     

    Can I export my libraries from 5.4.0 and re-import them into 4.16r1?

     

    Or even copy them?

     

    Thanks

     

    Robert

     

     

    On Fri, 13 Mar 2009 10:30:01 -0400, Brownie <nomail00@worldpath.net>

    wrote:

     

    Klaus Schmidinger wrote:

     

    On 03/13/09 05:15, Robert Lewis wrote:

    I found the problem; this is not Eagle at all but Windows XP. The

    problem was when I did a file operation such as search for a directory

    inorder to open a new schematic or to save a schematic or board. The

    error is

    " Event 8003

    The master browser has received a server announcement from the

    computer nnnn-PC that believes that it is the master browser for the

    domain on transport NetBT_Tcpip_{50BFAA9C-4CFA-44FE-B. The master

    browser is stopping or an election is being forced." Then the file

    operation fails, probably due to a network connection check and

     

    then Eagle terminates. I think Eagle should do a check on the return

    status from a file operation and not exit but notify and continue. A

    more graceful method in my estimation.

     

    Actually we do check the return codes of all file operations, so

    I wouldn't know what to change in that area.

     

    Are you getting any more specific error messages? Something that

    could indicate a problem in EAGLE?

     

    Klaus Schmidinger

     

    Hi Klaus and all

     

    Firstly we are all probably in the Wrong area for Bug discussion, but to

    keep the thread unbroken I return this comment here. Previous reply is

    above - Brownie - with system details.

     

    I just installed 5.4.4 and decided that since the Win system should always

    be rebooted after any software install - even if it does no Registry

    entry - we should run through a system cleanup - delete Junk Files.

     

    In looking under the root there was a File000.chk.  These are generated when

    there has been a system scan done - usually after some crash and reboot.

     

    We looked at the files with X-Tree Gold (very old Dos file manager that one

    must use with extreme caution under Win) binary viewer.  Both of the files

    were orphaned BUT complete files (based on the file sizes compared to Good

    files in the Project folder) generated from Eagle.  I'm sure that Eagle

    does NOT leave Loaded Files OPEN as some windows programs do.  There for my

    only best guess is that Eagle may have been trying to do an Auto-Save when

    Win took it's vacation.  This may fall in line with Mr. Lewis's comment

    above here.

     

    I hope this provides some insight Klaus.  This problem has happened several

    times over the last couple of months while running Eagle.  It may fall in

    line with some conversation we had several months ago regarding Win Crashes

    while doing Manual File Saves.

     

    Win does perform sporadic disk writes of it's own - anyone know why?

     

    Maybe this problem is so unpredictable because it's'  such a crap shoot to

    know if Win is about to do a disk write.  I don't think Win cares what else

    is going on so there could be some conflict if programs that do writes

    don't delay a bit if Win is busy.  Just a long-shot Guess.

     

    Thanks for allowing me the privilege to express my hopefully not too

    ignorant viewpoint.

     

    Regards All,

    Brownie

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • blewis999
    blewis999 over 17 years ago

    Unfortunately, Eagle 5.4.0 just terminated again but this time there

    are no events in the system log.

     

    I am not sure what to do... I do not have any other app's terminating.

    I just upgraded from Eagle 4.16r1 and have never had that version

    crash. I used 4.16r1 up to the time I installed 5.4.0 without problem

    and did no system upgrades between the install of 5.4 and using 4.16.

     

    Can I export my libraries from 5.4.0 and re-import them into 4.16r1?

     

    Or even copy them?

     

    Thanks

     

    Robert

     

     

    On Fri, 13 Mar 2009 10:30:01 -0400, Brownie <nomail00@worldpath.net>

    wrote:

     

    Klaus Schmidinger wrote:

     

    On 03/13/09 05:15, Robert Lewis wrote:

    I found the problem; this is not Eagle at all but Windows XP. The

    problem was when I did a file operation such as search for a directory

    inorder to open a new schematic or to save a schematic or board. The

    error is

    " Event 8003

    The master browser has received a server announcement from the

    computer nnnn-PC that believes that it is the master browser for the

    domain on transport NetBT_Tcpip_{50BFAA9C-4CFA-44FE-B. The master

    browser is stopping or an election is being forced." Then the file

    operation fails, probably due to a network connection check and

     

    then Eagle terminates. I think Eagle should do a check on the return

    status from a file operation and not exit but notify and continue. A

    more graceful method in my estimation.

     

    Actually we do check the return codes of all file operations, so

    I wouldn't know what to change in that area.

     

    Are you getting any more specific error messages? Something that

    could indicate a problem in EAGLE?

     

    Klaus Schmidinger

     

    Hi Klaus and all

     

    Firstly we are all probably in the Wrong area for Bug discussion, but to

    keep the thread unbroken I return this comment here. Previous reply is

    above - Brownie - with system details.

     

    I just installed 5.4.4 and decided that since the Win system should always

    be rebooted after any software install - even if it does no Registry

    entry - we should run through a system cleanup - delete Junk Files.

     

    In looking under the root there was a File000.chk.  These are generated when

    there has been a system scan done - usually after some crash and reboot.

     

    We looked at the files with X-Tree Gold (very old Dos file manager that one

    must use with extreme caution under Win) binary viewer.  Both of the files

    were orphaned BUT complete files (based on the file sizes compared to Good

    files in the Project folder) generated from Eagle.  I'm sure that Eagle

    does NOT leave Loaded Files OPEN as some windows programs do.  There for my

    only best guess is that Eagle may have been trying to do an Auto-Save when

    Win took it's vacation.  This may fall in line with Mr. Lewis's comment

    above here.

     

    I hope this provides some insight Klaus.  This problem has happened several

    times over the last couple of months while running Eagle.  It may fall in

    line with some conversation we had several months ago regarding Win Crashes

    while doing Manual File Saves.

     

    Win does perform sporadic disk writes of it's own - anyone know why?

     

    Maybe this problem is so unpredictable because it's'  such a crap shoot to

    know if Win is about to do a disk write.  I don't think Win cares what else

    is going on so there could be some conflict if programs that do writes

    don't delay a bit if Win is busy.  Just a long-shot Guess.

     

    Thanks for allowing me the privilege to express my hopefully not too

    ignorant viewpoint.

     

    Regards All,

    Brownie