Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Connect vias in bottom plane, and increasing supply to smd pads
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 187 subscribers
  • Views 843 views
  • Users 0 members are here
  • smd
  • pcb
  • vias
  • question
Related

Connect vias in bottom plane, and increasing supply to smd pads

vebjornr
vebjornr over 11 years ago

2 questions:

1) how do i connect these two segments? (see pic) The vias have the same name as the net. but when i try to use the routing-tool in the bottom plane, it automatically pops back up to the top plane..

 

2) How to i increase the thickness of the "legs" that connect the smd solder pads, to the rest of the ground-plane? (also see pic)

 

image

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 26/09/14 17:59, Vebjørn Røed Myklebust wrote:

    2 questions:

    1) how do i connect these two segments? (see pic) The vias have the same

    name as the net. but when i try to use the routing-tool in the bottom

    plane, it automatically pops back up to the top plane..

     

    Which end are you starting from? The end of the airwire towards the top

    of the image doesn't come from the via, so starting there will be forced

    onto the top layer. Try routing from the other via, or using

    click. You may still need to re-select bottom after you start

    routing, but normally you shouldn't as long as Eagle knows you're

    starting from a via.

     

    2) How to i increase the thickness of the "legs" that connect the smd

    solder pads, to the rest of the ground-plane? (also see pic)

     

    The automatic connections to a polygon are formed at the wire width of

    the polygon, I think. Edit the properties of your ground plane polygon

    to have a sensible width.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 26/09/14 17:59, Vebjørn Røed Myklebust wrote:

    2 questions:

    1) how do i connect these two segments? (see pic) The vias have the same

    name as the net. but when i try to use the routing-tool in the bottom

    plane, it automatically pops back up to the top plane..

     

    Which end are you starting from? The end of the airwire towards the top

    of the image doesn't come from the via, so starting there will be forced

    onto the top layer. Try routing from the other via, or using

    click. You may still need to re-select bottom after you start

    routing, but normally you shouldn't as long as Eagle knows you're

    starting from a via.

     

    2) How to i increase the thickness of the "legs" that connect the smd

    solder pads, to the rest of the ground-plane? (also see pic)

     

    The automatic connections to a polygon are formed at the wire width of

    the polygon, I think. Edit the properties of your ground plane polygon

    to have a sensible width.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to autodeskguest

    On 27/09/2014 6:24 a.m., Rob Pearce wrote:

    On 26/09/14 17:59, Vebjørn Røed Myklebust wrote:

    2 questions:

    1) how do i connect these two segments? (see pic) The vias have the same

    name as the net. but when i try to use the routing-tool in the bottom

    plane, it automatically pops back up to the top plane..

     

    Which end are you starting from? The end of the airwire towards the top

    of the image doesn't come from the via, so starting there will be forced

    onto the top layer. Try routing from the other via, or using

    <ctrl>click. You may still need to re-select bottom after you start

    routing, but normally you shouldn't as long as Eagle knows you're

    starting from a via.

     

    2) How to i increase the thickness of the "legs" that connect the smd

    solder pads, to the rest of the ground-plane? (also see pic)

     

    The automatic connections to a polygon are formed at the wire width of

    the polygon, I think. Edit the properties of your ground plane polygon

    to have a sensible width.

     

     

     

    I see there is another problem with the Element14 front end to the

    EagleCad forums.

     

    Rob wrote "click" and only "click" is displayed by Element14.

    Fingers crossed that the double quotes in this message will assist here.

     

    Warren