EAGLE User Support (English) What name and values get printed on silk screen?
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 178 subscribers
  • Views 877 views
  • Users 0 members are here
  • values
  • silk
  • screen
  • component
Related

What name and values get printed on silk screen?

Former Member
Former Member over 11 years ago

I'm using Eagle 7.1.0 on Windows. I have a board designed that I'd like to send for production, but I am not sure what actually is printed on the silk screen layer.

 

In my schematic view I have selected components (diodes, transistors, resistors...) from the libraries that have the symbol and footprint that I want used, and then I edited the values to have the mfg part numbers that will actually be used. For example, for a diode I selected BAS40 from the library because the footprint is for a SOT23 package, and then edited the value to be BZX84C6V2L because this is the diode that I will solder on the board - but I cannot find a library component for it.

 

The schematic values are displayed on the TSilk layer (I think) and as you see in the screen shot attachment the value text I added is used. I'm OK if this is printed, but if you look at the capacitor's value text it is very long and extends beyond the board edge.

 

My questions are:

  1) Will those values I've added actually be printed on the silk screen?

  2) How about the names, such as D1, C1, R1..., will they print?

  3) If they do print, is it possible to turn some off, but leave the value associated with the component in the schematic?

 

Thanks, I appreciate your help.

 

Bob

 

image

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    I'm the OP. I found this link, so I think maybe all my questions are answered, if not I'll reply again.

     

    http://www.element14.com/community/message/29880/l/re-silkscreen-help#29880

     

    Bob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago

    I'm the OP. I found this link, so I think maybe all my questions are answered, if not I'll reply again.

     

    http://www.element14.com/community/message/29880/l/re-silkscreen-help#29880

     

    Bob