EAGLE User Support (English) Questions on Eagle before sending a board off for production.
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
  • State Not Answered
  • Replies 5 replies
  • Subscribers 181 subscribers
  • Views 493 views
  • Users 0 members are here
Related

Questions on Eagle before sending a board off for production.

Former Member
Former Member over 11 years ago

Hi Jorge, et. al.

 

I have produced a PCB and have sent it for check at a board house and they said all is ok. Before committing I wanted to ensure success. Eagle reports 345 errors that are all in TStop layer. The solder mask crosses the silkscreen in many places, however, there is not much I can do about this, it is a tight layout. I have seen some videos on Eagle by Jeremy Blum where he states that most board houses will clean these up and to not worry about those errors.

 

Should I be concerned or not? I have limited experience and don't want to wait a month to receive defective boards! Your collective thoughts are appreciated in advance.

 

Below is an example:

image

  • Sign in to reply
  • Cancel
  • RayA
    0 RayA over 11 years ago

    I'm not an expert, but here's my take on it.

     

    1) The easy way would be to ask the board house to "clip" the silkscreen. Then they will automatically delete any portion of the silkscreen that interferes with exposed copper or open soldermask areas. In this case you can just "accept" the DRC errors.

     

    2) The better, but more time consuming way would be to delete the offending silkscreen areas manually, yourself. From the image that you included, it looks like you might need to open the library and edit the component. The "tPlace" layer can have silkscreen that DOES NOT cover up copper. This is what will print on the board. And the "tDocu" layer can have the complete silkscreen image. This is what you can print out on paper for the assembly drawing.

     

    Good luck.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to RayA

    On 21/10/14 01:49, RayA wrote:

    2) The better, but more time consuming way would be to delete the

    offending silkscreen areas manually, yourself. From the image that you

    included, it looks like you might need to open the library and edit the

    component. The "tPlace" layer can have silkscreen that DOES NOT cover up

    copper. This is what will print on the board. And the "tDocu" layer can

    have the complete silkscreen image. This is what you can print out on

    paper for the assembly drawing.

     

    While that's a good principle, and I would certainly encourage everyone

    to design their libraries such that nothing on tPlace overlaps any pads,

    once you get to the final board layout there are likely to be at least a

    few vias that sit under the component outline sections on the xPlace

    layers. This can't be fixed in the library in any meaningful manner.

     

    Most board houses will clip the silkscreen.

     

    On one occasion, though, I had a batch of boards where they had

    erroneously clipped the top silkscreen using the bottom mask, resulting

    in a couple of fragments printed onto copper. The boards all worked fine

    anyway, although that's more by luck than judgement.

     

    Cheers,

    Rob

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    In my experience, most board houses are good about removing silkscreen that

    impinges on pads.

    Most of them. Their manufacturing software will automatically look at

    places where silkscreen is over top of a pad, and sometimes over top of a

    place where there won't be soldermask (tStop/bStop).

     

    Some rough patches I've seen:

    - In EAGLE, there is the rectangle tool, which can be used in some

    libraries to show the location of pads or just simple rectangles.

    Silkscreen rectangles created with this tool can be treated differently by

    some older CAM packages, and they will be incapable of removing that

    silkscreen automatically. I've had that happen already where there was

    silkscreen covering a solderable pad. The board shop did remake the boards

    correctly at their expense, but it was still an inconvenience for me.

    Simple silkscreen lines and polygons are typically removed more

    consistently.

    - Other board shops with old CAM software implement an inefficient

    workaround: Their workers manually remove all unwanted silkscreen. Manual

    processes like this can leave the door open to errors.

     

    Board shops with newer or better CAM software are capable of very

    effectively and consistently removing silkscreen from solderable areas,

    including rectangles.

     

     

    Some board fab shops will always send you a checkplot or Gerbers to be

    approved before starting any production. You can ask for that on your order

    though:

    "Please send PDF checkplots  for approval before starting production of this order."

     

    The PDF checkplots I've received from my employer's primary board vendor

    are typically PDF format, with one board layer shown per page.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • engswee
    0 engswee over 11 years ago

    Dear J Chop,

     

    Everything should be fine. Unless it a mistake from your design and layout.

    For PCB making, they normally will not use this layer.

     

    If you don't want to see this error just deactivated them before run the DRC check.

    This will make your life easy with just few major error to check normally.

     

    Have Fun and Enjoys.

     

    Cheers,

    ES

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago

    Thanks all, I appreciate the information :-)