EAGLE User Support (English) Analog Electronics
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
  • State Not Answered
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 311 views
  • Users 0 members are here
Related

Analog Electronics

Former Member
Former Member over 11 years ago

Hello i am designing a operational amplifier, the project is to design an operational amplifier block to be used in a complex system-on-a-chip (SoC). I can either use a CMOS process from TSMC 0.35um HV CMOS technology, or a bipolar process from an unidentified foundary. The design must meet the requirements and it should be optimized for robustness, power, and/or speed. The design project is an opamp with the following characteristics: Gain>=60dB, Unity Gain frequency>=60MHz, Phase Margin>=45Deg, Offset<=50uV, Dynamic Rage =+/-6.5V (for 10mv error), Slew Rate>=80 V/us. The power supply is +/-7.5V. I need to know if Eagle can simulate all of the characteristics. I have my amplifier already mapped out with the values that i need i just need to simulate it. Is this possible?

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 11 years ago

    Hello Adrian,

     

    Is this a commercial or  a student project.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 11 years ago

    Hello Adrian,

     

    Is this a commercial or  a student project.

     

    MK