Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) No error reported on via in vrestrict (layer43) polygon !
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 907 views
  • Users 0 members are here
Related

No error reported on via in vrestrict (layer43) polygon !

kikoun
kikoun over 11 years ago

Hi,

 

On some package I add a vRestric (layer 43) polygon because I want to be sure that there will be no via (or holes) in this area.

But it seems that when I put a via in the area, there is no DRC error or warning !!!!

How can I activate this checking ???? (I hope it's possible !)

I already activate the 'Check restrict' in 'Misc' tab in the DRC setting.

 

Guillaume Barrey 

  • Sign in to reply
  • Cancel
Parents
  • kikoun
    0 kikoun over 11 years ago

    No body have a clue ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kikoun
    0 kikoun over 11 years ago

    No body have a clue ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to kikoun

    Guillaume barrey[1

    wrote on Wed, 05 November 2014 02:52]No body have a clue ?

     

     

    EAGLE won't give you an error if a via is placed in a rectangle or other

    shape on that layer.  All it does is restrict the auto-router from placing

    a via in that layer.

     

    Of course that is silly and really negates the point of the layer. 

    CadSoft should change this, or at least give an option for the vrestrict

    layer to actually create an error if a via is within that area.  That is

    what any rational person would think it does and it's actually a needed

    function.

     

    From the help for the RECT command

     

     

    If used in the layers tRestrict, bRestrict, or vRestrict, the RECT command

    defines restricted areas for the Autorouter.

     

     

    This isn't 100% true.  For tRestrict and bRestrict it will also create DRC

    errors if there is copper in those areas.  But vRestrict works differently.

    This is a bug and should be fixed.

     

    In addition, there is probably more nuanced control that is needed for

    blind and buried vias.  If you're trying to make sure that a via wouldn't

    short to the bottom of a connector (for instance) then it's OK if you have

    a via in that location as long as it doesn't come out to the surface.

     

    And while we're at it, being able to identify a restrict area on an inner

    layer is often needed as well.  For instance, under the antenna of an RF

    module.  Some nuance here because you'd want to put that into the footprint

    of a part to cover all layers but not all boards have all layers.  So that

    needs to be considered.

     

    So in general, I'd like to see a lot more improvement in the restrict

    methodology.  But yes, at a bare minimum vRestrict should give DRC errors

    when a via is placed in that area.

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

     

    Take advantage of v7 License Promotion right now at

    http://www.eaglecentral.ca

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer