EAGLE User Support (English) PCB Schematic with Philips Rebel LEDs
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
  • State Not Answered
  • Replies 9 replies
  • Subscribers 181 subscribers
  • Views 833 views
  • Users 0 members are here
Related

PCB Schematic with Philips Rebel LEDs

Former Member
Former Member over 11 years ago

Hey guys,

 

   I am relatively new to EagleCAD & PCB design, but I am doing a pretty basic board layout with some Philips Rebel LEDs. I am in the schematic layout for these LEDs, & have connected all of my +/- leads. Every time I go to do the ERC, I get a "No Supply for Power pin BLUE1TH TH" where BLUE1 is the name that I assigned to the LED. I used the invoke command to pull out a "hidden" thermal pin for each LED, but I have no idea where to connect them. Any advice?

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • kjames4
    0 kjames4 over 11 years ago

    I built a board with Philips Luxeon LEDs and the thermal pad contact to the ground plane.  The board works and the "isolated" claim for the thermal pad seems correct.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to kjames4

    So late last night I added a "TH" ground-connection to all the thermal pins of the LEDS. Then on the board layout I connected all these "TH" connections to a bottom layer ground/thermal plane. All the errors went away! The only question is, did I do this correctly? Guess I will get the board made & find out...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Workshopshed
    0 Workshopshed over 11 years ago in reply to Former Member

    Electrically this should not be a problem because thermal pad is isolated. So it's all about if you've put down enough copper to disipate the heat generated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Workshopshed

    If I want to make a metal core PCB on eagle cad, how do I distribute the layers. Do I just tell my board house that I want a certain layer to be aluminum?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kjames4
    0 kjames4 over 11 years ago in reply to Former Member

    The ground plane covers most of the back of my board, so there's a fair amount of copper.  I placed a cut-out in the ground plane solder mask behind the LEDs so I can make a good connection to a heat sink, but I haven't used one yet.  With 3 LEDs at full power (about 6W total supply) the contact area gets quite hot to the touch.  I wouldn't be comfortable running it that way for an extended time but heat does not seem excessive.  I expect a modest heat sink to do the job.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kjames4
    0 kjames4 over 11 years ago in reply to Former Member

    The ground plane covers most of the back of my board, so there's a fair amount of copper.  I placed a cut-out in the ground plane solder mask behind the LEDs so I can make a good connection to a heat sink, but I haven't used one yet.  With 3 LEDs at full power (about 6W total supply) the contact area gets quite hot to the touch.  I wouldn't be comfortable running it that way for an extended time but heat does not seem excessive.  I expect a modest heat sink to do the job.