EAGLE User Support (English) Font and text size changes when frame placed in drawing
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 177 subscribers
  • Views 308 views
  • Users 0 members are here
Related

Font and text size changes when frame placed in drawing

trainingsystems
trainingsystems over 11 years ago

Hi

I have just set up a new drawing Frame library part that matches (as near as possible) our approved company CAD drawing borders.

 

When I print out the library part everything looks OK but when I place this frame into a drawing the text font and sizes change so that text overflows boxes and looks poor.

 

Why does the frame change from the library part? I have used proportional for the font as this is the only one that looks anything like a normal Drawing Border font.

 

Is there any way to use a specific windows font in Eagle or just the fixed types already in the templates?

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 11/6/2014 11:23 AM, Richard Clayton wrote:

    Hi

    I have just set up a new drawing Frame library part that matches (as

    near as possible) our approved company CAD drawing borders.

     

    When I print out the library part everything looks OK but when I place

    this frame into a drawing the text font and sizes change so that text

    overflows boxes and looks poor.

    Keep in mind that if you have always show Vector font on, the

    proportional font will change to vector. On the board layout, Vector

    type font is the only type of font supported by the Gerber standard, so

    if you want a realistic view of the finished board on the layout you

    should use Vector font.

     

    Why does the frame change from the library part? I have used

    proportional for the font as this is the only one that looks anything

    like a normal Drawing Border font.

     

    Is there any way to use a specific windows font in Eagle or just the

    fixed types already in the templates?

    Only the three types of fonts that ship with EAGLE can be used.

     

    hth,

    Jorge Garcia

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 11/6/2014 11:23 AM, Richard Clayton wrote:

    Hi

    I have just set up a new drawing Frame library part that matches (as

    near as possible) our approved company CAD drawing borders.

     

    When I print out the library part everything looks OK but when I place

    this frame into a drawing the text font and sizes change so that text

    overflows boxes and looks poor.

    Keep in mind that if you have always show Vector font on, the

    proportional font will change to vector. On the board layout, Vector

    type font is the only type of font supported by the Gerber standard, so

    if you want a realistic view of the finished board on the layout you

    should use Vector font.

     

    Why does the frame change from the library part? I have used

    proportional for the font as this is the only one that looks anything

    like a normal Drawing Border font.

     

    Is there any way to use a specific windows font in Eagle or just the

    fixed types already in the templates?

    Only the three types of fonts that ship with EAGLE can be used.

     

    hth,

    Jorge Garcia