EAGLE User Support (English) help needed in determining materials list
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
  • State Suggested Answer
  • Replies 20 replies
  • Answers 2 answers
  • Subscribers 179 subscribers
  • Views 1831 views
  • Users 0 members are here
  • raspberry
  • management
  • pi
  • power
Related

help needed in determining materials list

mstng_67
mstng_67 over 11 years ago

Hello. I am very new to hardware development and am in need of some professional help determining what parts I need to accomplish my goal. I am looking to build a power management system for use inside a car. The system will be used to manage power to a Raspberry Pi. Attached is an accurate (yet I'm sure very crude...please pardon my ignorance) representation of what I'm trying to accomplish. The goal of this is to maintain a constant stream of clean power to the RasPi while the vehicle is in operation. Could I get some guidance on what materials I need in order to make this a success?

image

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 11 years ago

    I didn't understand the exact requirement, did you intend the RPI to gracefully power off when the vehicle is not in operation?

    If so, there are alternate ways that do not require the LiPo and step-up DC-DC converter - the sleepy pi would then likely meet the need.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mstng_67
    0 mstng_67 over 11 years ago in reply to shabaz

    Well, that's part of it. I also want to ensure no vehicle battery drain when the system is not in use. In addition, I need some mechanism to ensure the RPi is getting clean power in the hostile power environment present in a car. That was the thought behind the LiPO. The LiPO is meant to ensure a clean stream of power to the RPi no matter what the power condition is in the vehicle.

     

    The requirements are:

     

    1) Ensure that the system can completely power off such that there is not drain on the automotive battery.

    2) Ensure a clean and steady power supply to the RPi.

    3) Provide a mechanism to allow the RPi to shut itself down gracefully and then "wake up" when the vehicle key is switched to the "run" position. Note the IGN wire in my drawing. That's what starts the whole process.

     

    The sleepy pi may be an option. I am unsure if it the entire system can be completely shut down...meaning does the arduino stay powered on the whole time? If so, that would cause a drain on the automotive battery. Lastly, I see that it provides the power management I'm looking for; however, I really need to be able to fend off the spikes, brownouts, and sustained voltage craziness in the vehicle. I would still need some kind of battery to provide the consistent power I'm looking for...correct?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mstng_67
    0 mstng_67 over 11 years ago in reply to shabaz

    I have been experiencing power-related problems with my RPi project. Log messages harvested from the SD card suggest power-related issues that cause a bunch of horrible things to happen like the network interface to stop functioning. Over and over again I have come to realize that the RPi seems to be sensitive to in-vehicle power fluctuations. This is the largest impediment to my project. If I'm wrong, do you have any ideas what I may be experiencing and why? For example, when the RPi is running off of the vehicle battery and the vehicle is started, the only LED on the Pi that lights up is the second one and it stays red. Nothing else happens. The device will not function until I completely pull the power for several seconds and then re-apply power.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to mstng_67

    Regarding

    " however, I really need to be able to fend off the spikes, brownouts, and sustained voltage craziness in the vehicle. "

    You'd have to do that with any circuit intended for a vehicle, it is not eliminated using a LiPo - you have merely moved the problem to the input of the LiPo charger circuitry.

     

    By the way, 17V (the max input rating for the Sleepy Pi board) is quite low for vehicle use, so perhaps you may want to use a linear regulator (e.g. a 10V linear regulator like a LM7810) preceeding it.

    It wouldn't consume enough current in shutdown to worry about in a vehicle (about 6mA with typical linear regulators).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to shabaz

    On 06/11/14 22:09, shabaz wrote:

    Regarding

    " however, I really need to be able to fend off the spikes, brownouts,

    and sustained voltage craziness in the vehicle. "

    You'd have to do that with any circuit intended for a vehicle, it is not

    eliminated using a LiPo - you have merely moved the problem to the input

    of the LiPo charger circuitry.

     

    Vehicle electrical systems are a horrid environment, but just throwing a

    LiPo at it isn't the solution.

     

     

    By the way, 17V (the max input rating for the Sleepy Pi board) is quite

    low for vehicle use,

     

    Low but probably just about tolerable, as long as it's the max steady

    voltage. There will be momentary spikes above that. Mind you, I once

    encountered a (very expensive, German made) explicitly automotive piece

    of development kit that would fry a tantalum if subjected to over 16V

    for a fraction of a second.

     

    so perhaps you may want to use a linear regulator

    (e.g. a 10V linear regulator like a LM7810) preceeding it.

     

    I'd go with a series resistor and MOV rather than a (potentially equally

    sensitive) linear regulator

     

    It wouldn't consume enough current in shutdown to worry about in a

    vehicle (about 6mA with typical linear regulators).

     

    Most OEMs now consider 6mA an unacceptably high quiescent current for

    (an individual piece of) automotive electronics.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to shabaz

    Hi Shabaz, yeah the proposal is some what over complicated. Also the relays would be too slow switching the power to and from the Pi so really the LiPo would be redundant.

     

    I would suggest using a 5V 1-2A Switching regulator with  an inhibit/enable pin to control it powered directly from the permanent 12V.

     

    you would then need to work on the logic in such away that if the IGN 12V isn't present then the Regulator is inhibited thus will not switch on. This will need to have a bypass probably based on say a 555 monostable which is periodically reset by the RPI's GPIO.

     

    A script running will keep the power on after the key is removed only long enough to shut down cleanly....Voila!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to autodeskguest

    Hi Rob,

     

    That's a great idea, something like a 2.2R 2W would be great if the 17V is a bit too close for comfort (I didn't check to see what device the sleepy pi board uses), and a varistor as you say.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to Problemchild

    Hi John,

     

    Exactly, I agree, it was unnecessary complications!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to autodeskguest

    The sort of cheap Switching Reg I was thinking of will go to around 35V which I think is good enough for most situations in a car.

    I know if the alternator is running and the  battery is removed you can get spikes higher but that really is a fringe case.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Problemchild

    Several things to consider (vehicle power systems are notoriously noisy).

    The first thing I like to do is use a resistor in series with a diode in

    the supply (with a cap after it) to help provide isolation from the spikes

    - the resistor limits the current from the spike and the diode prevents

    reverse flow if bad things happen in the vehicle (like reversed battery)).

    You also need to consider signal conditioning on any other connections

    (sensors etc.) - spikes on those lines will also cause strange things for

    your board.  You not only need to make sure the power to the board is

    clean, but that all other connections to the board are also protected -

    lots of things generate spikes in that environment and lots of magnetic

    pulses (starter etc.) that can induce strange information into sense/data

    lines.  Running a processor in that environment is NOT trivial and you need

    to put lots of protection on all connections, not just the power.

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to Problemchild

    We've not even asked what he wants to do and we are engineering the finer points of the design.

    Can  Arch Nemesis explain what he wants to achieve with the Raspberry Pi in the car?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Problemchild

    On 8/11/2014 10:37 a.m., John Alexander wrote:

    We've not even asked what he wants to do and we are engineering the

    finer points of the design.

    Can  Arch Nemesis explain what he wants to achieve with the Raspberry Pi

    in the car?

    h5.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/130595

     

     

     

    And another thing. This is the support forum for the Cadsoft Eagle

    software.

     

    This is totally the wrong place for this discussion. Please take it

    elsewhere.

     

    Thank you

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Problemchild

    On 8/11/2014 10:37 a.m., John Alexander wrote:

    We've not even asked what he wants to do and we are engineering the

    finer points of the design.

    Can  Arch Nemesis explain what he wants to achieve with the Raspberry Pi

    in the car?

    h5.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/130595

     

     

     

    And another thing. This is the support forum for the Cadsoft Eagle

    software.

     

    This is totally the wrong place for this discussion. Please take it

    elsewhere.

     

    Thank you

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mstng_67
    0 mstng_67 over 11 years ago in reply to autodeskguest

    I am very sorry. I completely missed where this was. Is it possible for an admin to move this to the appropriate place?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to mstng_67

    Just ask Element14jamie to move it or just ask the question again

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to Problemchild

    The link doesn't work. however the project sounds very interesting. Please re ask the question on the Raspberry PI forum.

    I for one would like to  see what you are intending for your project. Please send us a link to the question.

    Better still start a blog post and get some points for it image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mstng_67
    0 mstng_67 over 11 years ago in reply to Problemchild

    Just ask Element14jamie to move it or just ask the question again

     

    image

     

    Thanks for the tip. However, I ran into a problem. Since Element14jamie is not following me, I can't PM him. See the attached photo. Any ideas?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to mstng_67

    Good question I asked someone who will hopefully pass it on .