EAGLE User Support (English) Ground fill area problem
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
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 178 subscribers
  • Views 525 views
  • Users 0 members are here
  • fill
  • polygons
Related

Ground fill area problem

Former Member
Former Member over 11 years ago

I have a question about fill areas.  I have noticed that if I want to have a fill area over an entire board, such as a ground plane, I can place a polygon around the board and name it something like "EarthG" and it works fine.  The fill will surround the pads and traces properly.  However, If I have any other filled areas on the board like just around a few pads, the fill area for the ground goes directly over the other fills without any regards to being different names.  Why?  The only way I've found to avoid this is to manually use traces to fill in the areas I want filled in and then the larger surrounding fill will avoid those areas.

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 11 years ago +1
    On 11/19/2014 2:20 PM, David Burghard wrote: I have a question about fill areas. I have noticed that if I want to have a fill area over an entire board, such as a ground plane, I can place a polygon around…
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 11/19/2014 2:20 PM, David Burghard wrote:

    I have a question about fill areas.  I have noticed that if I want to

    have a fill area over an entire board, such as a ground plane, I can

    place a polygon around the board and name it something like "EarthG" and

    it works fine.  The fill will surround the pads and traces properly.

    However, If I have any other filled areas on the board like just around

    a few pads, the fill area for the ground goes directly over the other

    fills without any regards to being different names.  Why?  The only way

    I've found to avoid this is to manually use traces to fill in the areas

    I want filled in and then the larger surrounding fill will avoid those

    areas.

     

    Hi David,

     

    I hope you're doing well. They short out, because by default all

    polygons have the same rank. The key to getting the polygons to separate

    is to use a different rank for the two or more polygons. A rank of 1 is

    the highest priority while 6 is  the lowest priority. In your example

    the internal polygon would have a rank of 1 and the big polygon would

    have a rank of two.

     

    The rank can be adjusted by looking at the properties of the polygon.

     

    Best Regards,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 11/19/2014 2:20 PM, David Burghard wrote:

    I have a question about fill areas.  I have noticed that if I want to

    have a fill area over an entire board, such as a ground plane, I can

    place a polygon around the board and name it something like "EarthG" and

    it works fine.  The fill will surround the pads and traces properly.

    However, If I have any other filled areas on the board like just around

    a few pads, the fill area for the ground goes directly over the other

    fills without any regards to being different names.  Why?  The only way

    I've found to avoid this is to manually use traces to fill in the areas

    I want filled in and then the larger surrounding fill will avoid those

    areas.

     

    Hi David,

     

    I hope you're doing well. They short out, because by default all

    polygons have the same rank. The key to getting the polygons to separate

    is to use a different rank for the two or more polygons. A rank of 1 is

    the highest priority while 6 is  the lowest priority. In your example

    the internal polygon would have a rank of 1 and the big polygon would

    have a rank of two.

     

    The rank can be adjusted by looking at the properties of the polygon.

     

    Best Regards,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to autodeskguest

    "Jorge Garcia"  skrev i nyhetsmeldingen: m4ivhf$vkg$1@cheetah.cadsoft.de ...

    They short out, because by default all polygons have the same rank.

     

    I see this question over and over again, and I'm thinking, wouldn't it be

    nice if the inner polygon always got render priority?

    Only in case of partly overlapping polygons, the need for the rank parameter

    would come up.

    (ps:cross posted to suggest.eng)

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    Thank you for the help.  It does seem, however, that no matter the 'ranking', polygons should be treated just like the routes and pads in that they are all named somehow, regardless of 'ranking' and should, therefore be avoided by other fill areas that have different names.  Seems like this should have been taken care of in version 1 instead of having to manually rank things.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Former Member

    On 11/20/2014 3:11 PM, David Burghard wrote:

    OK, so you are saying that right now the program won't allow me to

    manually change the ranking of the polygons right?

    Hi David,

     

    Unfortunately, not right. You can change polygon rank at any point in

    time. Just use the info command and click on one of the edges of the

    polygon. In the properties dialog, you'll see a parameter called Rank

    and you can adjust to the appropriate value.

     

    hth,

    Jorge Garcia

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    Sorry,

    I was responding to your system that emailed me only the last part of the conversation.  I tried to edit my response, which you did get, but it obviously also sent you this too.  I saw that I had not read the entire discussion and so this was sent in eror.

     

    Thanks again for the help.

     

    David Burghard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Former Member

    On 22/11/2014 3:51 a.m., David Burghard wrote:

    Sorry,

    I was responding to your system that emailed me only the last part of

    the conversation.  I tried to edit my response, which you did get, but

    it obviously also sent you this too.  I saw that I had not read the

    entire discussion and so this was sent in eror.

     

    Thanks again for the help.

     

    David Burghard

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/132463

     

     

     

     

    Element14 users should be aware that only E14 users will see the edits.

    Edits cannot update the forum post at the Cadsoft Forum.

     

    Warren