EAGLE User Support (English) Grid preventing propper wiring
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
  • State Verified Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 179 subscribers
  • Views 544 views
  • Users 0 members are here
  • wiring
  • grid
Related

Grid preventing propper wiring

Former Member
Former Member over 11 years ago

Two problems, actually:

 

 

  1. Whatever I set on grid options never sticks after restarting the program (I need grid Size to be 1 mm on the schematic - Don't know exactly what Multiple and Alt stand for);
  2. Wiring/Net insist on connecting on the grid vertices instead of the component pins (I did place the components after changing the grid);

 

Ctrl+Move snaps the component, but changes nothing.

 

 

How to fix this ?

 

 

 

Eagle 6.4.0

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    Lucas Silva wrote:

    2. Wiring/Net insist on connecting on the grid vertices instead of the

    component pins (I did place the components after changing the grid);

     

    Ctrl+Move snaps the component, but changes nothing.

     

    The pin of the symbols need to be on grid in the schematic editor.

    The default libraries are all designed for a 100mil grid.

     

    If you switching the schematic to a 1mm grid none of the default

    libraries will work properly.

     

     

    May I ask, why you think to need the 1mm grid in the schematic?

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    @"If you switching the schematic to a 1mm grid none of the default

    libraries will work properly."

     

    Now that's what I call bad software design.

     

     

     

    I need mm because of the components
    They are displayed in mm on the Add component browser

    And their dimensions (like length) are important. Even more important are the distances between pads of different components (I use the grid to locate myself).

     

     

    And last, but not least important: of around 192 countries in the world, I heard only tree of them use inch instead of mm. One is Mianmar (which I don't have a single idea of what continent it sits on).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kikoun
    0 kikoun over 11 years ago in reply to Former Member

    Hi,

     

    I agree that inch is less and less used in the world, and it's a good thing to use mm.

    In all my board I use a mm grid.

    But on schematic, I never change the grid, because of updating all the symbol.

    I don't understand why the dimension on pad components is important in your SCHEMATIC ? In you board, Yes I understand but in schematic nobody care about distance since it's symbolic representation (nothing to do with the real form of the component !!!!)

    Guillaume.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to kikoun

    You're right
    You're right...


    That's a big detail I did not realize: The schematic is not the actual board.

    That changes everything

     

    Feeling dumb right now
    image

     

     


    And on the board the grid works.

     

    Not perfectly, but it works.

     

    Thanks


    It's my fifth project, but only now units came to my concern.

     

    Only rests me to suggest the developers to take more care on units matters.

    Not changing big things, like the library, but other areas (whether it IS Incoherent to show mm on the component library and make it's model with mils)

     

    Even after changing the units I don't get integer values for Via widths, for example...

    Not cool.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Myanmar aka Burma

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Myanmar aka Burma