Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) SD Slot??
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 189 subscribers
  • Views 1038 views
  • Users 0 members are here
  • b+
  • on
  • pi
  • rasberry
  • slot
  • starter
  • kit
  • sd
Related

SD Slot??

e14 Contributor
e14 Contributor over 11 years ago

I am not sure if you can help me with this question or not but i just received the Rasberry pi B+ starter kit & i have put the pi into the case & see all the ports they explain on the "Getting Started Video" but i do not see a slot anywhere for the SD card? They said the card hold specific programs needed to boot the Pi. I am more than likely missing where it goes. Perhaps it is something that goes into my Personal pc slot or laptop? If you can help i would appreciate. Thanks

  • Sign in to reply
  • Cancel
Parents
  • packrat
    0 packrat over 11 years ago

    Hi Jessica,

     

    Check out the image guidoeagle links to, the board on the right is a B+ which has a micro sd slot. The starter kit comes with a 4GB micro SDHC card in it. About 15mm x 11m with a ''notch" at the bottom.   It also comes with a micro to full sized SD adapter (SD/SDHC/SDXC).

     

    The adapter lets you use the micro sd card in a full sized slot, like most PC's have.  Looking at the image, the board in the middle shows the adapter with a micro sd card inserted.  The notch at the bottom is used to remove it.

     

    Check yours, most likely you'll find the micro card hidden in the SD adapter.

     

    Walt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • packrat
    0 packrat over 11 years ago

    Hi Jessica,

     

    Check out the image guidoeagle links to, the board on the right is a B+ which has a micro sd slot. The starter kit comes with a 4GB micro SDHC card in it. About 15mm x 11m with a ''notch" at the bottom.   It also comes with a micro to full sized SD adapter (SD/SDHC/SDXC).

     

    The adapter lets you use the micro sd card in a full sized slot, like most PC's have.  Looking at the image, the board in the middle shows the adapter with a micro sd card inserted.  The notch at the bottom is used to remove it.

     

    Check yours, most likely you'll find the micro card hidden in the SD adapter.

     

    Walt