EAGLE User Support (English) Directory option no longer working?
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
  • State Verified Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 180 subscribers
  • Views 1712 views
  • Users 0 members are here
Related

Directory option no longer working?

matterama
matterama over 11 years ago

Hi all,

 

Using the Professional version...7.2...

 

I have a separate library folder that I point to with each new version of Eagle.  After a upgrade, the stock eagle directories are listed in "Options->Directories".  I typically remove this path and replace it with the path to my library folder.

 

As of 7.2, removing the eagle source libraries from the path does not work anymore.  When I go to "add" a part, I have duplicate libraries showing up.   This greatly slows everything down.

 

Can anyone else confirm this behavior and suggest a fix?  I have two machines that this runs on, both show the same problem...

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    For what it's worth in my case, win7/64 Eagle 6.5 - in my Directories

    settings for the libraries, I have

    "$EAGLEDIR\lbr;$HOME\eagle\mjf_lbr;$HOME\eagle\3rd_lbr" - when I select

    "Add" for a component, it does show all the libraries, but as I noted in my

    original post,

     

    If you activate the UPDATE command without a parameter, a file dialog will

    be presented to select the library from which to update."

    Unfortunately, if I do it that way, it does not give me the option of

    selecting my library. It appears to only offer libraries that are in the

    main lbr folder, not any other (like the ones in my personal path) in spite

    of the fact that in the "Directories" dialog, I do have the additional

    paths specified ( $EAGLEDIR\lbr;$HOME\eagle\mjf_lbr;$HOME\eagle\3rd_lbr )

    and the libraries are marked as active (green dot). I can see them from the

    libraries tree and use the parts, but the update dialog only shows the ones

    in the lbr tree, not in the "mjf_lbr" or "3rd_lbr" folders. Am I missing

    something or is this a bug? (Library Update all does pick up the changes so

    it knows to look there).  It is only looking in the default library, none

    of those listed in the Directories option.

     

    I did discover that while my libraries are NOT listed in the update option

    (although it can find them for parts doing an add), that if I look in the

    library tree I can RIGHT click my library and select "Update" and that

    seems to work also.

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago

    For what it's worth in my case, win7/64 Eagle 6.5 - in my Directories

    settings for the libraries, I have

    "$EAGLEDIR\lbr;$HOME\eagle\mjf_lbr;$HOME\eagle\3rd_lbr" - when I select

    "Add" for a component, it does show all the libraries, but as I noted in my

    original post,

     

    If you activate the UPDATE command without a parameter, a file dialog will

    be presented to select the library from which to update."

    Unfortunately, if I do it that way, it does not give me the option of

    selecting my library. It appears to only offer libraries that are in the

    main lbr folder, not any other (like the ones in my personal path) in spite

    of the fact that in the "Directories" dialog, I do have the additional

    paths specified ( $EAGLEDIR\lbr;$HOME\eagle\mjf_lbr;$HOME\eagle\3rd_lbr )

    and the libraries are marked as active (green dot). I can see them from the

    libraries tree and use the parts, but the update dialog only shows the ones

    in the lbr tree, not in the "mjf_lbr" or "3rd_lbr" folders. Am I missing

    something or is this a bug? (Library Update all does pick up the changes so

    it knows to look there).  It is only looking in the default library, none

    of those listed in the Directories option.

     

    I did discover that while my libraries are NOT listed in the update option

    (although it can find them for parts doing an add), that if I look in the

    library tree I can RIGHT click my library and select "Update" and that

    seems to work also.

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    Interesting and I have encountered similar bugs.  Today I downloaded libraries from Element14 and extracted to element14 subfolder.  I looked at the tree and saw TWO identical element14 folders the 2nd being in another library folder.  So I deleted that element14 folder and when I refreshed the tree items in BOTH element folders were gone.  So maybe I lost my work files same way by having two project folders with the same name (I intended to make a subfolder with same name as I wanted to work in the new folder and delete the original folder.)  Now I noticed I have two ltspice libraries, one is Libraries\ltspice and the other is Libraries\lbr\ltspice.  Don't know how that happened.