EAGLE User Support (English) Directory option no longer working?
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
  • State Verified Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 179 subscribers
  • Views 1682 views
  • Users 0 members are here
Related

Directory option no longer working?

matterama
matterama over 11 years ago

Hi all,

 

Using the Professional version...7.2...

 

I have a separate library folder that I point to with each new version of Eagle.  After a upgrade, the stock eagle directories are listed in "Options->Directories".  I typically remove this path and replace it with the path to my library folder.

 

As of 7.2, removing the eagle source libraries from the path does not work anymore.  When I go to "add" a part, I have duplicate libraries showing up.   This greatly slows everything down.

 

Can anyone else confirm this behavior and suggest a fix?  I have two machines that this runs on, both show the same problem...

 

Thanks!

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 11 years ago

    Greetings,

     

    I have similar but catastrophic using "Options->Directories".  I created New folder under Projects, then created .sch and .brd designs there, then created empty New library under Libraries.  But then my projects New folder was DELETED along with my .sch and .brd files.  The missing files are not on my hard drive and not in recycle bin.  This goofy directory management doesn't seem to work and I am very frustrated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    I wonder if this ties in with what I was seeing in version 6.5 that I asked

    about recently (

    http://www.eaglecentral.ca/forums/index.php/t/50419/263197e281ad9469b2edb50517b0c717/

    ) where the library update command only presents a list of libraries to

    work with in the original library path, but not any of the ones listed in

    the supplemental path(s) set in the "Directories" options (although at

    least in my case it hasn't deleted files for me !)

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 12/21/2014 12:30 PM, Matt Ryan wrote:

     

    Hi Matt,

     

    I hope you're doing well. Could you provide some more details about your

    operating system and any other pertinent details. I would appreciate

    similar info from others on this thread. This is the first I hear of

    such and issue.

     

    Additionally, a step by step procedure of how you ran into this bug will

    be helpful. There could be something in the sequence that causes the hickup.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    For what it's worth in my case, win7/64 Eagle 6.5 - in my Directories

    settings for the libraries, I have

    "$EAGLEDIR\lbr;$HOME\eagle\mjf_lbr;$HOME\eagle\3rd_lbr" - when I select

    "Add" for a component, it does show all the libraries, but as I noted in my

    original post,

     

    If you activate the UPDATE command without a parameter, a file dialog will

    be presented to select the library from which to update."

    Unfortunately, if I do it that way, it does not give me the option of

    selecting my library. It appears to only offer libraries that are in the

    main lbr folder, not any other (like the ones in my personal path) in spite

    of the fact that in the "Directories" dialog, I do have the additional

    paths specified ( $EAGLEDIR\lbr;$HOME\eagle\mjf_lbr;$HOME\eagle\3rd_lbr )

    and the libraries are marked as active (green dot). I can see them from the

    libraries tree and use the parts, but the update dialog only shows the ones

    in the lbr tree, not in the "mjf_lbr" or "3rd_lbr" folders. Am I missing

    something or is this a bug? (Library Update all does pick up the changes so

    it knows to look there).  It is only looking in the default library, none

    of those listed in the Directories option.

     

    I did discover that while my libraries are NOT listed in the update option

    (although it can find them for parts doing an add), that if I look in the

    library tree I can RIGHT click my library and select "Update" and that

    seems to work also.

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    Interesting and I have encountered similar bugs.  Today I downloaded libraries from Element14 and extracted to element14 subfolder.  I looked at the tree and saw TWO identical element14 folders the 2nd being in another library folder.  So I deleted that element14 folder and when I refreshed the tree items in BOTH element folders were gone.  So maybe I lost my work files same way by having two project folders with the same name (I intended to make a subfolder with same name as I wanted to work in the new folder and delete the original folder.)  Now I noticed I have two ltspice libraries, one is Libraries\ltspice and the other is Libraries\lbr\ltspice.  Don't know how that happened.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • matterama
    0 matterama over 11 years ago in reply to autodeskguest

    Hi Jorge,

     

    Your question has spawned new information...

     

    I am using version 7.2 and this happens on both a Win XP 32 bit and Win 7 64 bit platform.

     

    My options->directories library path has been modified to be simply:

    C:\Documents and Settings\Main User\My Documents\eagle\lbr

     

    I have copied the core libraries from the main Eagle directory to this folder, but also left them in the default directory.

     

    The original problem is:

    When, in a schematic, I type "add", then there is a long pause and when the add dialog comes up, it shows me entries for both the libraries located in my "My Documents" path and the main eagle path, despite the fact that the options->directories path is ONLY for the "My Documents" path.

     

    New information:

    I thought the duplicate path was the main eagle path, but it is not.  It is from the 7.1 version!!  So it is "C:\EAGLE-7.10/lbr/..."

     

    Help?  The 7.2 directory path is only to the My Documents lbr folder.  Why is it looking also in the older 7.1 version?

     

    Thanks,
    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to matterama

    I've never had anything but version 7.2.  Somehow folders with the same name become ghosts and deleting one deletes both.  That's how I lost my project files.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to matterama

    On 23/12/2014 3:18 p.m., Matt Ryan wrote:

    Hi Jorge,

     

    Your question has spawned new information...

     

    I am using version 7.2 and this happens on both a Win XP 32 bit and Win

    7 64 bit platform.

     

    My options->directories library path has been modified to be simply:

    C:\Documents and Settings\Main User\My Documents\eagle\lbr

     

    I have copied the core libraries from the main Eagle directory to this

    folder, but also left them in the default directory.

     

    The original problem is:

    When, in a schematic, I type "add", then there is a long pause and when

    the add dialog comes up, it shows me entries for both the libraries

    located in my "My Documents" path and the main eagle path, despite the

    fact that the options->directories path is ONLY for the "My Documents"

    path.

     

    New information:

    I thought the duplicate path was the main eagle path, but it is not.  It

    is from the 7.1 version!!  So it is "C:\EAGLE-7.10/lbr/..."

     

    Help?  The 7.2 directory path is only to the My Documents lbr folder.

    Why is it looking also in the older 7.1 version?

     

    Thanks,

    Matt

     

    If you are using projects the issue may be in the eagle.epf file of the

    project as it holds a list of the used libraries. Verify it by opening

    it in a text editor. If it does contain both 7.1 and 7.2 libraries that

    will be the cause of seeing both when you initiate an ADD.

     

    The easiest fix is to type USE -* in the command line. That will drop

    all libraries. Then USE the ones you want either from the control panel

    or use the command line again. See HELP > Editor Commands > USE

     

     

    HTH

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to matterama

    Hi Matt,

     

    Adding to Warren's comment, there's also the need to make sure that the

    eaglerc file is not being shared between multiple versions of EAGLE.

    This can create some "crosstalk" between versions. If you don't find

    that the EAGLE .epf file is the cause this is the next possible

    contender. This shouldn't be a problem in the V7 series but it's worth

    guaranteeing that it isn't a cause.

     

    I've found that the best way to handle this is to explicitly tell EAGLE

    what eaglerc file to use. This is done by starting EAGLE through a batch

    file. It's a simple one liner, here's mine:

     

    "C:\Program Files\EAGLE-6.5.0\bin\eagle.exe" -U"C:\Documents and

    Settings\Administrator\My Documents\eagle\eaglerc650.usr"

     

    Adjust the paths as necessary.

     

    hth,

    Jorge Garcia

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • matterama
    0 matterama over 11 years ago in reply to autodeskguest

    This did the trick Warren.  I've been upgrading like this from the 4.x series at least, never had the .usr file trump the project directory selection.  Thanks!

    Matt