EAGLE User Support (English) Directory option no longer working?
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
  • State Verified Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 180 subscribers
  • Views 1717 views
  • Users 0 members are here
Related

Directory option no longer working?

matterama
matterama over 11 years ago

Hi all,

 

Using the Professional version...7.2...

 

I have a separate library folder that I point to with each new version of Eagle.  After a upgrade, the stock eagle directories are listed in "Options->Directories".  I typically remove this path and replace it with the path to my library folder.

 

As of 7.2, removing the eagle source libraries from the path does not work anymore.  When I go to "add" a part, I have duplicate libraries showing up.   This greatly slows everything down.

 

Can anyone else confirm this behavior and suggest a fix?  I have two machines that this runs on, both show the same problem...

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 12/21/2014 12:30 PM, Matt Ryan wrote:

     

    Hi Matt,

     

    I hope you're doing well. Could you provide some more details about your

    operating system and any other pertinent details. I would appreciate

    similar info from others on this thread. This is the first I hear of

    such and issue.

     

    Additionally, a step by step procedure of how you ran into this bug will

    be helpful. There could be something in the sequence that causes the hickup.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • matterama
    0 matterama over 11 years ago in reply to autodeskguest

    Hi Jorge,

     

    Your question has spawned new information...

     

    I am using version 7.2 and this happens on both a Win XP 32 bit and Win 7 64 bit platform.

     

    My options->directories library path has been modified to be simply:

    C:\Documents and Settings\Main User\My Documents\eagle\lbr

     

    I have copied the core libraries from the main Eagle directory to this folder, but also left them in the default directory.

     

    The original problem is:

    When, in a schematic, I type "add", then there is a long pause and when the add dialog comes up, it shows me entries for both the libraries located in my "My Documents" path and the main eagle path, despite the fact that the options->directories path is ONLY for the "My Documents" path.

     

    New information:

    I thought the duplicate path was the main eagle path, but it is not.  It is from the 7.1 version!!  So it is "C:\EAGLE-7.10/lbr/..."

     

    Help?  The 7.2 directory path is only to the My Documents lbr folder.  Why is it looking also in the older 7.1 version?

     

    Thanks,
    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to matterama

    I've never had anything but version 7.2.  Somehow folders with the same name become ghosts and deleting one deletes both.  That's how I lost my project files.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to matterama

    I've never had anything but version 7.2.  Somehow folders with the same name become ghosts and deleting one deletes both.  That's how I lost my project files.