EAGLE User Support (English) Stopping TO-220 isolation
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
  • State Verified Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 179 subscribers
  • Views 806 views
  • Users 0 members are here
  • eagle
  • pcb
  • isolation
  • to-220
  • stop
Related

Stopping TO-220 isolation

Former Member
Former Member over 11 years ago

I have a problem which is keeping me working over the holiday -the only thing keeping my board from fab. image I've "tried everything" and read every Googled forum, but can't find the problem addressed (everyone wants to insulate their TO-220, not the other way around).

 

I have a 7805 in a TO-220 and I want the bolt hole connected directly to the ground plane ("GND") on the bottom (and the top). Eagle insists on isolating it. It seems Eagle has lots of ways to keep traces apart, but no ways to insist "I WANT COPPER HERE NO MATTER WHAT". I've edited the part, but to no avail; packages only have holes, not vias. I've even tried illegal ways, such as putting a hole on a via (didn't work). I've messed with all the DRC's (usually with bad consequences), but even that didn't fix it. If I can't solve this, I can always edit the Gerbers... p.s. NEVER had this problem with Bishop Graphics and Datak...


  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 25/12/2014 3:51 p.m., Steve Ins wrote:

    I have a problem which is keeping me working over the holiday -the only

    thing keeping my board from fab. image I've "tried everything" and read

    every Googled forum, but can't find the problem addressed (everyone

    wants to insulate their TO-220, not the other way around).

     

    I have a 7805 in a TO-220 and I want the bolt hole connected directly to

    the ground plane ("GND") on the bottom (and the top). Eagle insists on

    isolating it. It seems Eagle has lots of ways to keep traces apart, but

    no ways to insist "I WANT COPPER HERE NO MATTER WHAT". I've edited the

    part, but to no avail; packages only have holes, not vias. I've even

    tried illegal ways, such as putting a hole on a via (didn't work). I've

    messed with all the DRC's (usually with bad consequences), but even that

    didn't fix it. If I can't solve this, I can always edit the Gerbers...

    p.s. NEVER had this problem with Bishop Graphics and Datak...

     

     

    Hi. One way to do it, assuming you do not wish to create a four pin device.

     

    Make the library package a three pin device and ignore the tab as that

    will be your copper pour on the top and bottom layer. Also on a user

    defined layer mark the position where the screw hole should be located.

    This will be the location you place a via at on the board.

     

     

    When you edit the board, route pins 1 thru 3 normally.

    Place a via at the location you marked in the package. Name the via GND.

    Place your GND polygons and then RATSNEST.

     

    It should all look as you desire. The board house will make the screw

    hole a plated through via as there is copper top and bottom.

     

    HTH

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 25/12/2014 3:51 p.m., Steve Ins wrote:

    I have a problem which is keeping me working over the holiday -the only

    thing keeping my board from fab. image I've "tried everything" and read

    every Googled forum, but can't find the problem addressed (everyone

    wants to insulate their TO-220, not the other way around).

     

    I have a 7805 in a TO-220 and I want the bolt hole connected directly to

    the ground plane ("GND") on the bottom (and the top). Eagle insists on

    isolating it. It seems Eagle has lots of ways to keep traces apart, but

    no ways to insist "I WANT COPPER HERE NO MATTER WHAT". I've edited the

    part, but to no avail; packages only have holes, not vias. I've even

    tried illegal ways, such as putting a hole on a via (didn't work). I've

    messed with all the DRC's (usually with bad consequences), but even that

    didn't fix it. If I can't solve this, I can always edit the Gerbers...

    p.s. NEVER had this problem with Bishop Graphics and Datak...

     

     

    Hi. One way to do it, assuming you do not wish to create a four pin device.

     

    Make the library package a three pin device and ignore the tab as that

    will be your copper pour on the top and bottom layer. Also on a user

    defined layer mark the position where the screw hole should be located.

    This will be the location you place a via at on the board.

     

     

    When you edit the board, route pins 1 thru 3 normally.

    Place a via at the location you marked in the package. Name the via GND.

    Place your GND polygons and then RATSNEST.

     

    It should all look as you desire. The board house will make the screw

    hole a plated through via as there is copper top and bottom.

     

    HTH

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    Warren: I figure I could do it by making it 4-terminal, but that just seems so... yuk. Unfortunately, I could not get your method to work. On the board I am only allowed to place vias on layer "1-16", not on user-defined layers. At the package level, I cannot even create vias. Was this user-defined layer (i.e. layer 200) to be done at the package or board level? I tried placing a via directly under the bolt hole, but that overrode the bolt size and made the bolt hole the via diamater.