EAGLE User Support (English) Stopping TO-220 isolation
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
  • State Verified Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 179 subscribers
  • Views 803 views
  • Users 0 members are here
  • eagle
  • pcb
  • isolation
  • to-220
  • stop
Related

Stopping TO-220 isolation

Former Member
Former Member over 11 years ago

I have a problem which is keeping me working over the holiday -the only thing keeping my board from fab. image I've "tried everything" and read every Googled forum, but can't find the problem addressed (everyone wants to insulate their TO-220, not the other way around).

 

I have a 7805 in a TO-220 and I want the bolt hole connected directly to the ground plane ("GND") on the bottom (and the top). Eagle insists on isolating it. It seems Eagle has lots of ways to keep traces apart, but no ways to insist "I WANT COPPER HERE NO MATTER WHAT". I've edited the part, but to no avail; packages only have holes, not vias. I've even tried illegal ways, such as putting a hole on a via (didn't work). I've messed with all the DRC's (usually with bad consequences), but even that didn't fix it. If I can't solve this, I can always edit the Gerbers... p.s. NEVER had this problem with Bishop Graphics and Datak...


  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    I think from Eagle 6 upwards you can use the arbitrary pad shape

    function and just add a polygon to the gnd tab. The 4 pad device should

    work, just make sure when you create the part that in the connect dialog

    you connect Pad2 and the new ground tab pad 4 to the same GND pin in the

    schematic symbol.

     

    Merry Xmas

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago

    I think from Eagle 6 upwards you can use the arbitrary pad shape

    function and just add a polygon to the gnd tab. The 4 pad device should

    work, just make sure when you create the part that in the connect dialog

    you connect Pad2 and the new ground tab pad 4 to the same GND pin in the

    schematic symbol.

     

    Merry Xmas

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    Merry Xmas: It works, but it does make my library device specific to this PC board since it depends on how I routed around the pins, since the polygon must enclose the GND pin. It also gives "Package ... contains an invalid polygon." whenever I ratsnest.