EAGLE User Support (English) What is the difference between the wire tool and router tool in the layout?
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
  • State Not Answered
  • Replies 2 replies
  • Subscribers 179 subscribers
  • Views 879 views
  • Users 0 members are here
  • router
Related

What is the difference between the wire tool and router tool in the layout?

Former Member
Former Member over 11 years ago

After I used the autorouter on my design I was left with a couple of unrouted airwires which I had to route manually and that was okay. My problem started when I found a broken connection without any airwire (see the bottom of the picture). I might have deleted it without purpose. Since the airwire was gone I wasn't able to make a connection with the router. Will the wire tool work for routing? Or is it a way of routing where there is no airwires?

 

image

  • Sign in to reply
  • Cancel
  • dukepro
    0 dukepro over 11 years ago

    The difference is that the wire tool will simply place a copper wire on

    the board.  It will usually be given a name automatically as S$1, where

    the 1 would be replaced by the first unique value.  The route tool is

    used to route air wires into copper traces.  In this case, the traces

    produced inherit the name of the air wire.  I personally regard the wire

    tool as finger painting with copper.  I find rare use for it.

     

    As far as the broken connection in the image, the net may be connected

    elsewhere on the board, which would leave the two traces that are

    unconnected as stubs.  Another possibility is that an air wire exists

    for this broken connection, but not where you expect it.  The air wire

    will show up connecting the two closest vertexes on unconnected portions

    of the net.

     

    If you need to connect these at this point, click on the route tool,

    then do a Ctrl-Click on or near the end of the stub.

     

    HTH,

        - Chuck

     

     

    On 01/08/2015 01:31 PM, Simen Hexeberg wrote:

    After I used the autorouter on my design I was left with a couple of

    unrouted airwires which I had to route manually and that was okay. My

    problem started when I found a broken connection without any airwire

    (see the bottom of the picture). I might have deleted it without

    purpose. Since the airwire was gone I wasn't able to make a connection

    with the router. Will the wire tool work for routing? Or is it a way of

    routing where there is no airwires?

     

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/136862

     

     

    Attachments:
    1220.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 08/01/15 18:31, Simen Hexeberg wrote:

    After I used the autorouter on my design I was left with a couple of

    unrouted airwires which I had to route manually and that was okay. My

    problem started when I found a broken connection without any airwire

    (see the bottom of the picture). I might have deleted it without

    purpose. Since the airwire was gone I wasn't able to make a connection

    with the router. Will the wire tool work for routing? Or is it a way of

    routing where there is no airwires?

     

    Eagle doesn't let you "delete" a routed track, only rip it up. Assuming

    you're sure those orphan ends are supposed to be connected, the lack of

    airwire may mean Eagle thinks they are actually connected elsewhere.

    This happens often with ground and supply tracks, which get routed round

    the board so extensively that it's hard to spot by eye.

     

    The other possibility, which your image was too small to show, is that

    Eagle has found a point of closer approach elsewhere (perhaps where a

    connection really isn't practical) and shown the airwire there.

    Remember: airwires appear at the shortest possible straight line between

    two disconnected parts of the same net.

     

    If you have two tracks that are connected a long way away or have the

    airwire in the wrong place, you can route from where you want to by

    holding the  key down and clicking on the point on the wire.

     

    HTH

    Rob