EAGLE User Support (English) Eagle 5.5 Autoroute
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
  • Replies 13 replies
  • Subscribers 181 subscribers
  • Views 886 views
  • Users 0 members are here
Related

Eagle 5.5 Autoroute

Former Member
Former Member over 16 years ago

I have an existing board design that auto-routes fine with v5.4, but only

routes to 96% with v5.5

Same board... no changes.

 

This has forced me to revert back to v5.4

 

The board is fairly large (7.5x3.5 inches) with 1 100pin QLFP chip and a few

other 14/16pin SMT chips.

I have been using Eagle for several years with much more complex designs

(BGA,etc.) but I can't seem to get this fairly simple board to auto-route

with 5.5

 

Are there any settings in 5.5 that are more 'sensitive' than in 5.4?

 

Thanks

Peter

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

    Where can I find version 5.5.1?

     

     

    On 04/23/09 4:51 AM, Klaus Schmidinger wrote:

    On 04/23/09 10:13, Klaus Schmidinger wrote:

    On 04/22/09 18:22, pch wrote:

    I have an existing board design that auto-routes fine with v5.4, but only

    routes to 96% with v5.5

    Same board... no changes.

     

    This has forced me to revert back to v5.4

     

    The board is fairly large (7.5x3.5 inches) with 1 100pin QLFP chip and a few

    other 14/16pin SMT chips.

    I have been using Eagle for several years with much more complex designs

    (BGA,etc.) but I can't seem to get this fairly simple board to auto-route

    with 5.5

     

    Are there any settings in 5.5 that are more 'sensitive' than in 5.4?

    Looks like a bug has crept into version 5.5 that causes this.

    We're currently debugging it...

     

    Fixed for version 5.5.1.

     

    Klaus Schmidinger

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago

    Where can I find version 5.5.1?

     

     

    On 04/23/09 4:51 AM, Klaus Schmidinger wrote:

    On 04/23/09 10:13, Klaus Schmidinger wrote:

    On 04/22/09 18:22, pch wrote:

    I have an existing board design that auto-routes fine with v5.4, but only

    routes to 96% with v5.5

    Same board... no changes.

     

    This has forced me to revert back to v5.4

     

    The board is fairly large (7.5x3.5 inches) with 1 100pin QLFP chip and a few

    other 14/16pin SMT chips.

    I have been using Eagle for several years with much more complex designs

    (BGA,etc.) but I can't seem to get this fairly simple board to auto-route

    with 5.5

     

    Are there any settings in 5.5 that are more 'sensitive' than in 5.4?

    Looks like a bug has crept into version 5.5 that causes this.

    We're currently debugging it...

     

    Fixed for version 5.5.1.

     

    Klaus Schmidinger