EAGLE User Support (English) Traces showing over holes
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
  • State Not Answered
  • Replies 7 replies
  • Subscribers 180 subscribers
  • Views 1055 views
  • Users 0 members are here
Related

Traces showing over holes

Former Member
Former Member over 10 years ago

Hello,

 

I reinstalled windows and eagle recently, and now Eagle does something it didn't use to do before.

 

image

The holes are now covered with traces, and I don't like it.

 

Anyone maybe familiar with this problem? Thanks in Advance image

 

PS: Sorry if I made some mistakes, English is not my mother tongue.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 7/02/2015 9:05 a.m., Miloš Glendža wrote:

    Hello,

     

    I reinstalled windows and eagle recently, and now Eagle does something

    it didn't use to do before.

     

     

    The holes are now covered with traces, and I don't like it.

     

     

    You did not say which version of Eagle you are now using.

    You did not say how you arrived at the image you posted .

    .

    On v6.6 or v7.1 I don't see that issue when I print to a pdf

     

    HTH

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to autodeskguest

    Sorry, didn't think it was relevant.

     

    The version is 6.6.0.

     

    I do this:

     

    1) set palette white; ra

    2) display none bottom pad via; ra

    3) File >> Export >> Image (600 dpi, Monochrome) >> Ok

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • guidoeagle
    0 guidoeagle over 10 years ago in reply to Former Member

    Hello,

     

    when I export a layout as an image I get the same behaviour as you described in your first post (Eagle 6.6.5 & 6.6.0). Exporting a layout as an image is not the best way for pcb production in my opinion. Use the CAM-processor to export your layout. I know the CAM processor is not able to create images as raster graphics (*.png) but you can create a vector graphics in postscript (*.ps) format. This is anyway much better. Your local print house should be able to handle this format. Use ghostscript (http://ghostscript.com/) and ghostview (http://pages.cs.wisc.edu/~ghost/gsview/index.htm) to show *.ps-files on your computer.

     

    Best regards

    Guido

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to guidoeagle

    Actually it is (was) a great and easy way of creating images for toner transfer technique. I guess I'll check those things out, oh well. Thanks!

     

    EDIT: Installed Eagle 7.1, same thing. This really sucks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago in reply to guidoeagle

    Actually it is (was) a great and easy way of creating images for toner transfer technique. I guess I'll check those things out, oh well. Thanks!

     

    EDIT: Installed Eagle 7.1, same thing. This really sucks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • guidoeagle
    0 guidoeagle over 10 years ago in reply to Former Member

    On 07.02.2015 15:09, Miloš Glendža wrote:

    Actually it is (was) a great and easy way of creating images for toner

    transfer technique. I guess I'll check those things out, oh well.

    Thanks!

     

    Hello,

     

    it's not that complicated. Load your project and click on the

    CAM-Processor symbol in the tool bar of the board editor. In the

    CAM-Processor dialog click "File" => "Open" => "Job..." and load a cam

    job file (for example the one I've attached here). After that click on

    the "start job" button. After that you will find two postscript files in

    your project folder. The postscript file for the component side is named

    "*.cmp.ps", the postscript file for solder side is named "*.sol.ps".

     

    You can open these files with ghostview and convert them to raster

    graphic files ("File" => "Convert..."). But believe me, when you ever

    had worked with the vector graphics format you won't use the raster

    graphics format for your pcb layouts anymore.

     

    Best regards

    Guido

     

    P.S.: As I use a German eagle version the naming of the menu items and

    buttons might be slightly different as translated here.

    Attachments:
    8103.att1.html.zip
    MyCamJob.cam.zip