EAGLE User Support (English) Excellon CAM .drd files
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
  • Replies 4 replies
  • Subscribers 177 subscribers
  • Views 1905 views
  • Users 0 members are here
Related

Excellon CAM .drd files

autodeskguest
autodeskguest over 16 years ago

I am new to Eagle, so I am sure that I am doing something wrong.

 

I draw up a schematic.  I make the board.  Everything looks okay.  I use the

CAM Processor to make the Gerber files (gerb274x.cam).  I look at them using

the free edition of ViewMate (v10.4.32).  They look fine.

 

Here's the problem:  I use the CAM Processor to make the Drill Data files

(excellon.cam).  Whether I look at them through ViewMate or send them to my

board house's (Advanced Circuits / www.4pcb.com) Design for

Manufacturability check (www.freedfm.com), none of the holes line up with

the pads.  In fact, the holes are WAY off -- my board is 1.75" x 2", and the

holes are over in the 10" plus range and not to scale.

 

When I draw up the schematic in different software, the holes all line up.

What am I doing wrong.

 

Boyd

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

     

    "Philip Hodgers" <philip@puresoft.co.uk> wrote in message

    news:gt7eh4$7fa$1@cheetah.cadsoft.de...

    Here's the problem:  I use the CAM Processor to make the Drill Data files

    (excellon.cam).  Whether I look at them through ViewMate or send them to

    my board house's (Advanced Circuits / www.4pcb.com) Design for

    Manufacturability check (www.freedfm.com), none of the holes line up with

    the pads.  In fact, the holes are WAY off -- my board is 1.75" x 2", and

    the holes are over in the 10" plus range and not to scale.

     

    Note that EAGLE has a

    2.4 precision format and many Gerber viewers default to a 2.3 format so

    the

    scaling of the drills/holes is off. Just import in 2.4 precision for the

    drills/holes and all should be well, you'll need to advise this to the

    board house also.

     

    Regards, Philip Hodgers

     

    I am not so sure that that is the solution.  My other PCB software program

    used the 2.4 precision format, and it imported into ViewMate correctly.  I

    can't find where to change the precision in ViewMate (if it is even

    possible) -- I think it just accepts what you send it.

     

    Plus, if it is CAM'd at 2.4 and the Gerber files view correctly, why won't

    the Drill file?

     

    Boyd

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago

     

    "Philip Hodgers" <philip@puresoft.co.uk> wrote in message

    news:gt7eh4$7fa$1@cheetah.cadsoft.de...

    Here's the problem:  I use the CAM Processor to make the Drill Data files

    (excellon.cam).  Whether I look at them through ViewMate or send them to

    my board house's (Advanced Circuits / www.4pcb.com) Design for

    Manufacturability check (www.freedfm.com), none of the holes line up with

    the pads.  In fact, the holes are WAY off -- my board is 1.75" x 2", and

    the holes are over in the 10" plus range and not to scale.

     

    Note that EAGLE has a

    2.4 precision format and many Gerber viewers default to a 2.3 format so

    the

    scaling of the drills/holes is off. Just import in 2.4 precision for the

    drills/holes and all should be well, you'll need to advise this to the

    board house also.

     

    Regards, Philip Hodgers

     

    I am not so sure that that is the solution.  My other PCB software program

    used the 2.4 precision format, and it imported into ViewMate correctly.  I

    can't find where to change the precision in ViewMate (if it is even

    possible) -- I think it just accepts what you send it.

     

    Plus, if it is CAM'd at 2.4 and the Gerber files view correctly, why won't

    the Drill file?

     

    Boyd