EAGLE User Support (English) Excellon CAM .drd files
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
  • Replies 4 replies
  • Subscribers 177 subscribers
  • Views 1917 views
  • Users 0 members are here
Related

Excellon CAM .drd files

autodeskguest
autodeskguest over 16 years ago

I am new to Eagle, so I am sure that I am doing something wrong.

 

I draw up a schematic.  I make the board.  Everything looks okay.  I use the

CAM Processor to make the Gerber files (gerb274x.cam).  I look at them using

the free edition of ViewMate (v10.4.32).  They look fine.

 

Here's the problem:  I use the CAM Processor to make the Drill Data files

(excellon.cam).  Whether I look at them through ViewMate or send them to my

board house's (Advanced Circuits / www.4pcb.com) Design for

Manufacturability check (www.freedfm.com), none of the holes line up with

the pads.  In fact, the holes are WAY off -- my board is 1.75" x 2", and the

holes are over in the 10" plus range and not to scale.

 

When I draw up the schematic in different software, the holes all line up.

What am I doing wrong.

 

Boyd

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 16 years ago

    Here's the problem:  I use the CAM Processor to make the Drill Data files

    (excellon.cam).  Whether I look at them through ViewMate or send them to my

    board house's (Advanced Circuits / www.4pcb.com) Design for Manufacturability

    check (www.freedfm.com), none of the holes line up with the pads.  In fact,

    the holes are WAY off -- my board is 1.75" x 2", and the holes are over in the

    10" plus range and not to scale.

     

    Note that EAGLE has a

    2.4 precision format and many Gerber viewers default to a 2.3 format so the

    scaling of the drills/holes is off. Just import in 2.4 precision for the

    drills/holes and all should be well, you'll need to advise this to the board

    house also.

     

    Regards, Philip Hodgers

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 16 years ago

     

    "Philip Hodgers" <philip@puresoft.co.uk> wrote in message

    news:gt7eh4$7fa$1@cheetah.cadsoft.de...

    Here's the problem:  I use the CAM Processor to make the Drill Data files

    (excellon.cam).  Whether I look at them through ViewMate or send them to

    my board house's (Advanced Circuits / www.4pcb.com) Design for

    Manufacturability check (www.freedfm.com), none of the holes line up with

    the pads.  In fact, the holes are WAY off -- my board is 1.75" x 2", and

    the holes are over in the 10" plus range and not to scale.

     

    Note that EAGLE has a

    2.4 precision format and many Gerber viewers default to a 2.3 format so

    the

    scaling of the drills/holes is off. Just import in 2.4 precision for the

    drills/holes and all should be well, you'll need to advise this to the

    board house also.

     

    Regards, Philip Hodgers

     

    I am not so sure that that is the solution.  My other PCB software program

    used the 2.4 precision format, and it imported into ViewMate correctly.  I

    can't find where to change the precision in ViewMate (if it is even

    possible) -- I think it just accepts what you send it.

     

    Plus, if it is CAM'd at 2.4 and the Gerber files view correctly, why won't

    the Drill file?

     

    Boyd

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 16 years ago

    Boyd Nielsen schreef:

     

    "Philip Hodgers" <philip@puresoft.co.uk> wrote in message

    news:gt7eh4$7fa$1@cheetah.cadsoft.de...

    Here's the problem:  I use the CAM Processor to make the Drill Data

    files (excellon.cam).  Whether I look at them through ViewMate or

    send them to my board house's (Advanced Circuits / www.4pcb.com)

    Design for Manufacturability check (www.freedfm.com), none of the

    holes line up with the pads.  In fact, the holes are WAY off -- my

    board is 1.75" x 2", and the holes are over in the 10" plus range and

    not to scale.

     

    Note that EAGLE has a

    2.4 precision format and many Gerber viewers default to a 2.3 format

    so the

    scaling of the drills/holes is off. Just import in 2.4 precision for the

    drills/holes and all should be well, you'll need to advise this to the

    board house also.

     

    Regards, Philip Hodgers

     

    I am not so sure that that is the solution.  My other PCB software

    program used the 2.4 precision format, and it imported into ViewMate

    correctly.  I can't find where to change the precision in ViewMate (if

    it is even possible) -- I think it just accepts what you send it.

     

    Plus, if it is CAM'd at 2.4 and the Gerber files view correctly, why

    won't the Drill file?

     

    Boyd

     

    Well, I'm with Philip on this one. It likely is just a scaling problem.

    I use GC-Prevue to check the gerbers and it almost always get's the

    scaling wrong if i let it 'autoguess' (and the preview looks like you

    describe). If i specify the precision, while importing the excellon

    file, it's perfectly fine. My board house never seems to get 'confused'

    though, i get boards with drills where they belong image

     

    The problem is ONLY with the excellon file, not the other cam files,

    which use a different structure.

     

    Regards,

     

    Richard

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 16 years ago

    Thanks for both of your help.  Although my previewer was set to 2.4, there

    IS an import option that I could select ("All digits present") that allowed

    it to preview correctly:

     

        Zeros

            o    Omit trailing zeros

            o    Omit leading zeros

            .    All digits present

            o    Explicit decimal point

     

    Again, thank you,

    Boyd

     

    "Richard Herman" <postbus@het-audio-team.removethis.nl> wrote in message

    news:gt7stv$6sc$1@cheetah.cadsoft.de...

    Boyd Nielsen schreef:

     

    "Philip Hodgers" <philip@puresoft.co.uk> wrote in message

    news:gt7eh4$7fa$1@cheetah.cadsoft.de...

    Here's the problem:  I use the CAM Processor to make the Drill Data

    files (excellon.cam).  Whether I look at them through ViewMate or send

    them to my board house's (Advanced Circuits / www.4pcb.com) Design for

    Manufacturability check (www.freedfm.com), none of the holes line up

    with the pads.  In fact, the holes are WAY off -- my board is 1.75" x

    2", and the holes are over in the 10" plus range and not to scale.

     

    Note that EAGLE has a

    2.4 precision format and many Gerber viewers default to a 2.3 format so

    the

    scaling of the drills/holes is off. Just import in 2.4 precision for the

    drills/holes and all should be well, you'll need to advise this to the

    board house also.

     

    Regards, Philip Hodgers

     

    I am not so sure that that is the solution.  My other PCB software

    program used the 2.4 precision format, and it imported into ViewMate

    correctly.  I can't find where to change the precision in ViewMate (if it

    is even possible) -- I think it just accepts what you send it.

     

    Plus, if it is CAM'd at 2.4 and the Gerber files view correctly, why

    won't the Drill file?

     

    Boyd

     

    Well, I'm with Philip on this one. It likely is just a scaling problem. I

    use GC-Prevue to check the gerbers and it almost always get's the scaling

    wrong if i let it 'autoguess' (and the preview looks like you describe).

    If i specify the precision, while importing the excellon file, it's

    perfectly fine. My board house never seems to get 'confused' though, i get

    boards with drills where they belong image

     

    The problem is ONLY with the excellon file, not the other cam files, which

    use a different structure.

     

    Regards,

     

    Richard