I am new to Eagle, so I am sure that I am doing something wrong.
I draw up a schematic. I make the board. Everything looks okay. I use the
CAM Processor to make the Gerber files (gerb274x.cam). I look at them using
the free edition of ViewMate (v10.4.32). They look fine.
Here's the problem: I use the CAM Processor to make the Drill Data files
(excellon.cam). Whether I look at them through ViewMate or send them to my
board house's (Advanced Circuits / www.4pcb.com) Design for
Manufacturability check (www.freedfm.com), none of the holes line up with
the pads. In fact, the holes are WAY off -- my board is 1.75" x 2", and the
holes are over in the 10" plus range and not to scale.
When I draw up the schematic in different software, the holes all line up.
What am I doing wrong.
Boyd