Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) ULP: how to open a library when ULP was started in a schematic??
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 1655 views
  • Users 0 members are here
  • ulp
Related

ULP: how to open a library when ULP was started in a schematic??

Joop14
Joop14 over 11 years ago

Hello all,

 

I want to do something simple but somehow I can not find the right way or command.

 

I'm writing an ULP that is going to be started from a schematic.

In the ULP, I want to write code that opens a library so that I can access the properties of devices in a library.

 

How do I do this?

 

Kind Regards,

 

Joop

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 20/02/2015 5:35 a.m., Joop14 wrote:

    Hello all,

     

    I want to do something simple but somehow I can not find the right way

    or command.

     

    I'm writing an ULP that is going to be started from a schematic.

    In the ULP, I want to write code that opens a library so that I can

    access the properties of devices in a library.

     

    How do I do this?

     

    Kind Regards,

     

    Joop

     

     

    Hi

    I'm thinking  that you may get what you are after by right clicking the

    symbol in the schematic and selecting 'open device'. Running a ULP at

    that point is simpler. Explain more about you case. I'll write as much

    as you write.

     

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Joop14
    0 Joop14 over 11 years ago in reply to autodeskguest

    I'll explain a bit more what I want to try to achieve.

     

    I want to write an ULP that performs a diff between the parts/devices/footprints in a schematic/board and the libraries.

    In order to do this, the ULP must be started in the console of the schematic/board because we need to have access to all the parts/devices used in the schematic.

    Also we need to have access to all properties and attributes of these parts/devices.

     

    Once we have this access (which is easy when you start the ULP in the console of the schematic or board), we need to have access to

    the libraries to compare the properties of the parts in the schematic/board with the parts in the libraries.

     

    I can have access to parts and properties of a library when I start tyhe ULP in the console of a library.

     

    So, the question is, how to open a library from within an ULP that has been started in a schematic or board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Joop14

    On 20/02/2015 10:06 p.m., Joop14 wrote:

    I'll explain a bit more what I want to try to achieve.

     

    I want to write an ULP that performs a diff between the

    parts/devices/footprints in a schematic/board and the libraries.

    In order to do this, the ULP must be started in the console of the

    schematic/board because we need to have access to all the parts/devices

    used in the schematic.

    Also we need to have access to all properties and attributes of these

    parts/devices.

     

    Once we have this access (which is easy when you start the ULP in the

    console of the schematic or board), we need to have access to

    the libraries to compare the properties of the parts in the

    schematic/board with the parts in the libraries.

     

    I can have access to parts and properties of a library when I start tyhe

    ULP in the console of a library.

     

    So, the question is, how to open a library from within an ULP that has

    been started in a schematic or board.

     

     

    There are few ways to approach this:

     

    1. Using two ULPs.

      (a) Start the first in the schematic and gather all the required  info

        which you place in a file (my_file.txt)

      (b) Exit the first ulp which calls the second ulp.

       "Run 2nd_ULP my_file.txt"

    (c)Use my_file.txt to locate the library names/devices/symbols/packages

    of interest

    (d) compare the results

     

    2. Using 1 ULP

      This is the same as using two but all the code is in one ULP.

      (a) You sense when you are in the schematic and run that code portion.

      (b) Exit the first ulp which first opens the library editor and then

    calls itself in the library this time.

      (c) the library part of the code runs

     

    3.  Using 1 ULP - analyse the xml of the schematic which has all the

    device information and compare with the xml of the libraries

     

    I hope this gives you some ideas.

     

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to autodeskguest

    "warrenbrayshaw"  skrev i nyhetsmeldingen: mc7u3h$fq3$1@cheetah.cadsoft.de

    ...

    1. Using two ULPs.

     

    Just a minor comment to that.

    Of course you can do it all with one single ULP. It causes a tidyer ulp

    folder. You simply pass some self interpreting arguments via argv,argc.

    (Note:argv[0] is the ulp name itself so we can use this to rerun ourselves

    even if the ULP gets renamed):

    ---

    if(argc==2 and argv[1]="SecretKeywordToStartStage2")

    {

        //stage2

        exit(EXIT_SUCCESS);

    }

    else

    {

        //stage1

     

        sprintf(cmd,"dosomething;run %s SecretKeywordToStartStage2;",argv[0]);

        exit(cmd);

    }

    ---

     

    Also its good to know how to  access board and schematics from the same ulp

    by:

    ---

    if (project.board) project.board(B)

    {

    }

    if (project.schematics) project.schematics(S)

    {

    }

    ---

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Joop14
    0 Joop14 over 11 years ago in reply to autodeskguest

    Thanks Warren, your solution works.

    However, it wil not win a "beauty contest". It's more a kind of a hack.

    This is not your fault ofcourse. It's because of the limitations of Eagle & ULP.

     

    I'm not sure about the speed of opening and closing many different libaries (imagin you have a big design).

    Also, if an intermediate file is necessary to temporary store the properties of all the parts,

    why not just read directly from the xml files?

     

    So, I decided not to write an ULP. Instead, I'm going to write it in C.

    Thanks for the advice anyway.

     

    Joop

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Joop14
    0 Joop14 over 11 years ago in reply to autodeskguest

    Thanks Warren, your solution works.

    However, it wil not win a "beauty contest". It's more a kind of a hack.

    This is not your fault ofcourse. It's because of the limitations of Eagle & ULP.

     

    I'm not sure about the speed of opening and closing many different libaries (imagin you have a big design).

    Also, if an intermediate file is necessary to temporary store the properties of all the parts,

    why not just read directly from the xml files?

     

    So, I decided not to write an ULP. Instead, I'm going to write it in C.

    Thanks for the advice anyway.

     

    Joop