EAGLE User Support (English) TO92 alternative footprint
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
  • State Suggested Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 180 subscribers
  • Views 3560 views
  • Users 0 members are here
  • eagle
  • footprint
  • pcb
Related

TO92 alternative footprint

Former Member
Former Member over 11 years ago

I'm trying to add some BC547B transistors which is TO-92 package. This transistor, and any other TO-92 package I purchase from element 14 has the pins single in line (SIL).

 

image

However, seems all the transistors in the Eagle PCB libraries has a footprint of the older triangular layout of pins.

 

image

Being new to Eagle PCB I have no idea how to fix this. Trying to select any other PNP TO-92 transistors does not help as they all have the same footprint.

 

Can you please point me in the right direction (or library) I can use.

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 11 years ago in reply to Former Member +1
    On 5/03/2015 9:42 p.m., jengel wrote: Thank you shabaz for the reply. It would seem I'll have to go down the modified library path. Luckily I don't have to deal with forming machines. I am surprised though…
Parents
  • Former Member
    0 Former Member over 11 years ago

    Did you start with a schematic?

    As you say you are new to CADsoft, then go to the installation folder and find the DOC folder which contains 'tutorial' amd 'manual'.

    These files are great help.

     

    Mogens

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Yes, I did start with a schematic.

     

    I read through the documentation. Other than creating or modifying the library files, I don't see how to fix this.

    I downloaded the latest Fairchild Library and searched for the component using the element14 product code (1017673) to make I get the correct device. Still, the footprint does not match that of the datasheet or the actual device.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    From eagle library you can choose another NPN that has the footprint you want and then use the BC547 when you are ready to plug the transistors into the board.

    Good luck,

     

    Mogens

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Thanks, that will work for a small circuit as a work around but will result in a lot of manual updates to correct values and mess up the BOM for larger circuits.

     

    Is there a simple (a few clicks) way to correct the library by changing only the footprint, or is up to the supplier of the libraries to update?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Thanks, that will work for a small circuit as a work around but will result in a lot of manual updates to correct values and mess up the BOM for larger circuits.

     

    Is there a simple (a few clicks) way to correct the library by changing only the footprint, or is up to the supplier of the libraries to update?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 11 years ago in reply to Former Member

    Hi jengel,

     

    You can edit the library yourself if you like, and then select Library->Update in the schematic view to perform the update on all such parts in your schematic (and then manually correct any traces you may have already laid out in the PCB view).

    However, I think maybe PCB assembly/production may have forming machines for transistors? If this is for a personal project, the pins will be extremely close together, so perhaps it is better to use the existing footprint, and manually form the wires to fit?

    Anyway, you can edit the library if this is what you really want to do (but better to create your own library for custom parts like this). This is described in the EAGLE manual.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to shabaz

    Thank you shabaz for the reply.

     

    It would seem I'll have to go down the modified library path.

     

    Luckily I don't have to deal with forming machines. I am surprised though at how so many transistors can have the wrong footprint. I would have thought an application so popular (and expensive) would cater for the most common footprint.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Former Member

    On 5/03/2015 9:42 p.m., jengel wrote:

    Thank you shabaz for the reply.

     

    It would seem I'll have to go down the modified library path.

     

    Luckily I don't have to deal with forming machines. I am surprised

    though at how so many transistors can have the wrong footprint. I would

    have thought an application so popular (and expensive) would cater for

    the most common footprint. s

     

     

    I feel this straight leg (low cost) TO92 variant was never intended to

    be inserted without forming the legs.

     

    Have look at the dimensions

    http://www.onsemi.com/pub_link/Collateral/BC546-D.PDF

     

    Consider how small the lands will be once the hole size and clearance

    between pads is considered.

     

    HTH

    Warren

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    Good point, I never thought about the fact that I might have to bend it anyway.