Hi
A new user.
Using Eagle 7.2.0 Lite, how do I know if a new part has plated through holes? (as opposed to pads top and bottom).
Thanks
Hi
A new user.
Using Eagle 7.2.0 Lite, how do I know if a new part has plated through holes? (as opposed to pads top and bottom).
Thanks
Plated through holes are controlled by the rules of the board house.
Most commonly the board house will plate the hole if there is copper lands
on both sides of the board at the position of the drill.
If there is copper only on one side or neither side, the hole will be non
plated. That drilling occurs later in the manufacturing process. It pays to
learn the sequence of events in the manufacturer of a PCB then you can see
what is controlled by the CAD and what is controlled by the manufacturing
process.
You normally have to ask for a non plated hole if there is copper both
sides.
The board house will tell you how they wish to be advised of these needs.
HTH
Warren
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
The eagle primitives 'via' and 'pad' are always ment to be plated. For non
plated holes, there is the 'hole' primitive.
For course if you drill your own vias and pads, you have to make sure they
are connected at both top and bottom. If its a pad, it may be difficult to
actually solder the pin on both sides, but there is no such thing as a
bottom only pad in eagle. Maybe there should be since farnell/cadsoft does
seem to target the low entry users..
To keep those types of drills separated, I made my own CAM that creates
separate drillfiles for nonplated (holes) and plated (vias/pads). For some
reason eagle puts up a warning when I do that, but its very natural for me
to separate them and manufacturing house never complained.
The eagle primitives 'via' and 'pad' are always ment to be plated. For non
plated holes, there is the 'hole' primitive.
For course if you drill your own vias and pads, you have to make sure they
are connected at both top and bottom. If its a pad, it may be difficult to
actually solder the pin on both sides, but there is no such thing as a
bottom only pad in eagle. Maybe there should be since farnell/cadsoft does
seem to target the low entry users..
To keep those types of drills separated, I made my own CAM that creates
separate drillfiles for nonplated (holes) and plated (vias/pads). For some
reason eagle puts up a warning when I do that, but its very natural for me
to separate them and manufacturing house never complained.