EAGLE User Support (English) Is there anyway to exclude parts from the PCB
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
  • State Not Answered
  • Replies 29 replies
  • Subscribers 181 subscribers
  • Views 4342 views
  • Users 0 members are here
Related

Is there anyway to exclude parts from the PCB

Former Member
Former Member over 10 years ago

In Eagle Cad, is there anyway to exclude components on the schematic from the board view? I have several parts that will be wired to screw terminals. They still need to be shown in the schematic, but I do not need or want them on the board. I can't leave them outside the board area, so what's a guy to do? Thanks...

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 10 years ago +1
    On 3/26/2015 4:38 AM, Derek Tombrello wrote: In Eagle Cad, is there anyway to exclude components on the schematic from the board view? I have several parts that will be wired to screw terminals. They still…
  • autodeskguest
    autodeskguest over 9 years ago in reply to Former Member +1
    Mark Winters wrote: Hello Jorge. I wonder if you could point me to some documentation that helps me to remove the package as explained. I have made a copy of the component in my own library but return…
Parents
  • Former Member
    0 Former Member over 10 years ago

    it cannot become this still with the eagle
    do not wait for marvels from eagle


    read here
    http://www.element14.com/community/message/118034/l/re-beta-version-6911-available#118034

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to Former Member

    I know this is an Eagle forum, but is there any program (Linux) that CAN do this? Thanks for the reply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to Former Member

    I will bet that there is a file like XML which can be problematically changed if the layout is well known. But why would you want to do this? A simpler way would be labelling them optional. Or create separate views one with and one without. Just think "outside the box".image

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    "Outside the box"... if you were to see the circuit I am trying to build, you'd probably tell me to get back into the box! lol... I don't understand "label them optional" but I do have two schematics - one with and one without the components - but the problem with that is that if I make a modification to the circuit, I have to remember to update TWO schematics instead of just one. And my memory is NOT that great!

     

    Why would I want to? My current circuit has an off-board IR receiver-transmitter pair. Obviously, they are important to the circuit, so that have to be shown on the schematic, but since they are off-board, they do not need to be placed on the PCB view. It's like if you are designing an (admittedly old-school) amplifier. The volume control is panel mounted, so you don't need or want to have a footprint or pads for that on the PCB board, but it still needs to be in the schematic. Does that make sense?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    "Outside the box"... if you were to see the circuit I am trying to build, you'd probably tell me to get back into the box! lol... I don't understand "label them optional" but I do have two schematics - one with and one without the components - but the problem with that is that if I make a modification to the circuit, I have to remember to update TWO schematics instead of just one. And my memory is NOT that great!

     

    Why would I want to? My current circuit has an off-board IR receiver-transmitter pair. Obviously, they are important to the circuit, so that have to be shown on the schematic, but since they are off-board, they do not need to be placed on the PCB view. It's like if you are designing an (admittedly old-school) amplifier. The volume control is panel mounted, so you don't need or want to have a footprint or pads for that on the PCB board, but it still needs to be in the schematic. Does that make sense?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    Derek Tombrello wrote on Thu, 26 March 2015 22:14

    I don't understand "label them optional" but I do have two schematics -

    one with and one without the components - but the problem with that is

    that if I make a modification to the circuit, I have to remember to

    update TWO schematics instead of just one. And my memory is NOT that

    great!

     

    That is a case where I think the work flow of gEDA or Kicad is superior to

    EAGLE.  With either of those, it is a one-way trip, whereas EAGLE is

    two-way.  What I mean by that is that with gEDA and Kicad, you make a

    schematic with symbols, then you process that schematic to add the packages

    for the board, and then you do the layout.  If you want a different board

    (e.g. surface mount instead of through hole), you process the schematic

    again and make a separate layout.  If you make any changes to the

    schematic, you have to remember to go through the process again to

    propagate changes to the board, but at least you have only one schematic to

    maintain.

     

    EAGLE is a two-way process; they call it forward-backward annotation.  That

    ties the board back to the schematic, so that you can make certain changes

    in the board and the schematic gets updated.  I think this is a much better

    way of working on designs that have one schematic and one board, but it's

    not ideal for single schematics with multiple board layouts...

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to Former Member

    I see many designs in different groups making them easier to analyse. But I see the problem with two managing updates. Yikes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to Former Member

    Perhaps I'm missing something, but if you have a panel mounted volume

    control, you still need pads on the PCB to solder the wires that are

    soldered to the volume control.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.