EAGLE User Support (English) Is there anyway to exclude parts from the PCB
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
  • State Not Answered
  • Replies 29 replies
  • Subscribers 181 subscribers
  • Views 4365 views
  • Users 0 members are here
Related

Is there anyway to exclude parts from the PCB

Former Member
Former Member over 10 years ago

In Eagle Cad, is there anyway to exclude components on the schematic from the board view? I have several parts that will be wired to screw terminals. They still need to be shown in the schematic, but I do not need or want them on the board. I can't leave them outside the board area, so what's a guy to do? Thanks...

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 10 years ago +1
    On 3/26/2015 4:38 AM, Derek Tombrello wrote: In Eagle Cad, is there anyway to exclude components on the schematic from the board view? I have several parts that will be wired to screw terminals. They still…
  • autodeskguest
    autodeskguest over 9 years ago in reply to Former Member +1
    Mark Winters wrote: Hello Jorge. I wonder if you could point me to some documentation that helps me to remove the package as explained. I have made a copy of the component in my own library but return…
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    Jorge Garcia wrote:

    On 3/26/2015 4:38 AM, Derek Tombrello wrote:

    In Eagle Cad, is there anyway to exclude components on the schematic

    from the board view? I have several parts that will be wired to screw

    terminals. They still need to be shown in the schematic, but I do not

    need or want them on the board. I can't leave them outside the board

    area, so what's a guy to do? Thanks...

     

    Hi Derek,

    I hope you're doing well. This is possible. In the library for those

    components create an attribute with the name EXTERNAL. This tells

    EAGLE that this part is off board and therefore doesn't require a

    package on the board layout.

     

    In order for this to work the device can not have a package. So you may

    need to create a variant of those parts without packages.

     

    To do this I open the respective library and then in the control

    center right-click on the device-set I want to create the package-less

    variant off and copy to library.

    Eagle asks for a different name (because the device-set already

    existst); I append -NP (no package) to the original name.

     

    Now I open the new device-set, remove all packages and add the

    EXTERNAL property.

     

    Save the library and update the schematic.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to autodeskguest
    In short
    If for a such work, it needs transformation in the library or anything other time-consuming work
     
    It is easier to have two different schematic


    After all that you read, you understood that it is not in position the eagle it makes this work
    As well as other a lot of basic works
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago in reply to autodeskguest
    In short
    If for a such work, it needs transformation in the library or anything other time-consuming work
     
    It is easier to have two different schematic


    After all that you read, you understood that it is not in position the eagle it makes this work
    As well as other a lot of basic works