EAGLE User Support (English) internal part connection and routing
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
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 178 subscribers
  • Views 1001 views
  • Users 0 members are here
Related

internal part connection and routing

jonhpeterson
jonhpeterson over 10 years ago

eagle cad v 7.2.0

i have a part (didn't design it) with 3 pads and two pins:

add=next

swap=0

G$1.+ VCC@1 VCC@2

G$1.- GND

airwire and routing only to one of the VCC pads.

airwire will not go to the other VCC pad and routing to the other pad does not resolve the airwire.

I thought that either of the two pads should satisfy the routing and remove the airwire.

Does anyone have any ideas?

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    Jon Peterson wrote:

     

    eagle cad v 7.2.0

    i have a part (didn't design it) with 3 pads and two pins:

    add=next

    swap=0

    G$1.+ VCC@1 VCC@2

    G$1.- GND

    airwire and routing only to one of the VCC pads.

    airwire will not go to the other VCC pad and routing to the other pad

    does not resolve the airwire.

    I thought that either of the two pads should satisfy the routing and

    remove the airwire.

     

    In the device editor you can either use 'connect all' or 'connect any'

    to connect the pads to a pin.

     

    The former results in the layout editor showing air wires to all pads,

    the latter lets the editor be content with only one pad routed.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • jonhpeterson
    0 jonhpeterson over 10 years ago in reply to autodeskguest

    Had a little struggle with the command syntax. But got it to work. Big Thanks.

     

    Jon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jonhpeterson
    0 jonhpeterson over 10 years ago in reply to autodeskguest

    Had a little struggle with the command syntax. But got it to work. Big Thanks.

     

    Jon