EAGLE User Support (English) invert tstop bstop soldermask layer
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
  • State Suggested Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 181 subscribers
  • Views 1327 views
  • Users 0 members are here
  • invert
  • tstop
  • bstop
  • layer
  • soldermask
Related

invert tstop bstop soldermask layer

Former Member
Former Member over 10 years ago

Hi,

 

I want to design a two layer PCB as heating surface that is screwed against a heat exchanger. I plan to use lots of distributed SMD resistors with one pad on the ground plane (no thermals) and the other one connected through a via to Vcc. For technical reasons, I want to place the resistors on the side against the heat exchanger featuring a trench in which they are placed.

 

To make the heat transfer  uniform and efficient, I do not want to have a soldermask except a small  frame around the pad of the resistor. This way, the thick copper layer is pressed directly against the heatsink.

The ideal thing would be to be able to inverse the definition of the tstop layer: Directly draw the solder stop shapes, instead of defining  all the zones where no solderstop is allowed (as its typically done).

 

Is this possible? Or are there any good work arounds a PCB manufacturer can work with?

 

Many thanks!

  • Sign in to reply
  • Cancel
Parents
  • Joop14
    0 Joop14 over 10 years ago

    Create a polygon in layer 29 (tStop) with the size of the board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to Joop14

    Yes but thing is, cutout option for polygon doesn't seem to work on the tstop layer...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Joop14
    0 Joop14 over 10 years ago in reply to Former Member

    Quote from the manual: "Only polygons in signal layers can have the pour style "Cutout"."

     

    I wonder why...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Joop14
    0 Joop14 over 10 years ago in reply to Former Member

    Quote from the manual: "Only polygons in signal layers can have the pour style "Cutout"."

     

    I wonder why...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer