Hi all,
I have created a new device from scratch: a 60 pin connector.
This device has a tricky part: 6 pins are rounded pins with holes, so I have used SMD pads combined with polygons (to draw the holes) in order to follow datasheet drawings:
After drawing its simbol and package, I'm checking that is working properly in sch and brd files. In the schematic looks working fine. But I have noticed that in the board file the connections made in the schematic are not shown. You can see it in the next (example) image:
In the image above, is quite obvious that something is wrong with the connector: while I use standard devices, the rastsnets appear when I make a new wire, but nothing appears in the connector... I have checked the package: I have used SMD pads (first image);
Also the symbol, standard IO pins and device menu also looks fine...
Does anyone knows what I'm doing wrong???
Thanks in advance!!