EAGLE User Support (English) how to define non-signal (ground) layer in v7.2
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
  • State Verified Answer
  • Replies 25 replies
  • Subscribers 181 subscribers
  • Views 4531 views
  • Users 0 members are here
  • signal
  • 7.2
  • plane
  • non
  • ground
  • layer
Related

how to define non-signal (ground) layer in v7.2

Former Member
Former Member over 10 years ago

Using the standard version, with a top/bottom and 3 other routing inner layers, a very split power plane layer, how do I define a non-signal inner ground layer that can be polygon poured and get anti-pads around non-ground signal vias during ratsnest?

Stackup will be with only 6 signal layers (if you count the power plane):

1) Top with SMT, low frequency traces, and some high speed routing traces

2) desired inner ground layer

3) inner low frequency routing layer

4) Power plane

5) a 2nd copy of the inner ground layer

6) inner high frequency routing layer

7) inner high frequency routing layer

8) Bottom with SMT components...

Note that I'm going to be using TH vias rather than buried or blind vias, as well as some TH connectors

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 10 years ago

    Eagle advertises 6 signal layers in standard version.  How do I define non-signal board layer?

    Anyone willing to answer?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to Former Member

    Hi Bruce,

    In the display command you can click the ADD button to add non-signal
    layers.

    It can also be done from the command line with the LAYER command.

    Let me know if there's anything else I can do for you.

    Best Regards,
    Jorge Garcia

    Thank you Jorge. Posted here from official Eagle site.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to autodeskguest

    Whomever you are as a Cadsoft Guest, don't accuse me of either.  It is untrue.  You need to be polite.

    I disagree it (a ground layer or even another supply layer) is considered a signal by the industry in that it does not carry information.

    If Cadsoft wants to be as specific as saying 6 signal layers, and I understand they used to separately offer supply layers, then there should be some accommodation to continue to handle supply layers - which is what I'm asking for.

     

    Signal (electrical engineering)

     

    From Wikipedia, the free encyclopedia

     

    http://en.wikipedia.org/wiki/Signal_(electrical_engineering)#mw-headhttp://en.wikipedia.org/wiki/Signal_(electrical_engineering)#p-search

     

    This article is about signals in electrical engineering.

     

    A signal as referred to in communication systems, signal processing, and electrical engineering "is a function that conveys information about the behavior or attributes of some phenomenon".[1] In the physical world, any quantity exhibiting variation in time or variation in space (such as an image) is potentially a signal that might provide information on the status of a physical system, or convey a message between observers

    All About Circuits: "A signal is any kind of physical quantity that conveys information."

    Sparkfun:

    "Define: Signals

    Before going too much further, we should talk a bit about what a signal actually is, electronic signals specifically (as opposed to traffic signals, albums by the ultimate power-trio, or a general means for communication). The signals we’re talking about are time-varying “quantities” which convey some sort of information. In electrical engineering thequantity that’s time-varying is usually voltage (if not that, then usually current). So when we talk about signals, just think of them as a voltage that’s changing over time."

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to Former Member

    Hi,

    I think two, four and 6-layer PCB layout bundles are pretty standard. In electronic engineering the word 'signal' has a meaning, but in the PCB layout engineering world it is already (for decades?) very clear that software is offered typically licensed in two, four, six and unlimited number of copper layers. Where they are licensed in such a manner (as opposed to pin count for example) I don't think unlimited power planes are available for the 2, 4 and 6 layer offerings. I could be wrong.

    Here is a Cadstar page which offers the same number of layers, as does EasyPC for their routing product. These are just two random examples.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to shabaz

    Thank you for the further perspective.

    I have only been in the PCB Layout engineering world for a couple years and now getting into more than a couple board layers and BGA. 

    I obtained the "6 signal layer" license with the expectation of additional "supply layer"s that I saw referenced, since it used the term signal layer rather than copper or board layers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    Bruce Mellen wrote on Thu, 30 April 2015 17:43

    I obtained the "6 signal layer" license with the expectation of

    additional "supply layer"s that I saw referenced, since it used the term

    signal layer rather than copper or board layers.

     

    In all your pedantry, I think you're forgetting one thing.  Just because

    you know whether there is a signal on a copper layer doesn't mean that

    any CAD software "knows" whether there is a signal or not.  You can add a

    signal to something labeled "ground" as well as something labeled "+5V" if

    you want.  I don't see how you came up with the assumption that you could

    have as many copper layers as you wished as long as you knew there was no

    signal on them...

     

    My personal interpretation  of the literature is that CADSOFT provides 6

    signal layers as opposed to x number of graphic layers or dimension layers,

    etc.  IANAL

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to autodeskguest

    Reason: because supply layers have been described out here in addition to the signal layers.  Supply layers, which I understood would accept polygons but not traces.  I apparently misinterpreted, but Eagle could have been (or be) implemented as such:  Not allowing routing of signals on layers other than 6 chosen would effectively limit the software to 6 signal layers and additional desired supply layers (poured power and ground planes) that one can afford to have manufactured.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    Bruce Mellen wrote on Thu, 30 April 2015 18:45

    I apparently misinterpreted, but Eagle could have been (or be)

    implemented as such:  Not allowing routing of signals on layers other

    than 6 chosen would effectively limit the software to 6 signal layers and

    additional desired supply layers (poured power and ground planes) that

    one can afford to have manufactured.

     

    So, if you can afford to have these kinds of multi-layer boards

    manufactured, it would seem to me you could afford the ~$800 to upgrade to

    the Professional version of EAGLE...

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to autodeskguest

    Sadly not.  Perhaps someday with more experience and time, but it is just my very part time semi-retirement hobby that I'm getting into at this point, and a further upgrade is substantially beyond my budget.  I need what funds I have to prototype my experiments.  My experiments/prototypes will now have to experience the consequences of a lack of a pair of ground planes that would have been coupled to high speed routing layers and the power plane in the originally proposed question stackup.  From my reading, an 8 layer board is the first one that can do high speed routing and coupling correctly, while limiting EMI.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    Bruce Mellen prodded the keyboard with:

     

    From my reading, an 8 layer board is the

    first one that can do high speed routing and coupling correctly,

    while limiting EMI.

     

    Prior to retirement, I used to happily use three and four layer boards

    at 10 Ghz.

     

    --

    Best Regards:

                          Baron.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to autodeskguest

    My present ambitious goal involves a 1mm pitch 484 ball BGA, ddr3, and some high speed connectors to other  2/4 layer boards that do other things.  I feel the need to minimize all noise possible, given connectors to other things.

     

    Are you still doing anything related - just for fun?

    Feel free to contact me directly if more curious.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    Bruce Mellen prodded the keyboard with:

     

    My present ambitious goal involves a 1mm pitch 484 ball BGA, ddr3,

    and some high speed connectors to other  2/4 layer boards that do

    other things.  I feel the need to minimize all noise possible, given

    connectors to other things.

     

    With those sort of high density bga you might struggle with 6 layers.

    Crosstalk could also be an issue.

     

    Are you still doing anything related - just for fun?

    Feel free to contact me directly if more curious.

     

    No. I'm much happier not having to think about circuit design

    nowadays.  Wandering around europe is far nicer image

    Thanks for the invite anyway.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/148665

     

    --

    Best Regards:

                          Baron.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    Bruce Mellen prodded the keyboard with:

     

    My present ambitious goal involves a 1mm pitch 484 ball BGA, ddr3,

    and some high speed connectors to other  2/4 layer boards that do

    other things.  I feel the need to minimize all noise possible, given

    connectors to other things.

     

    With those sort of high density bga you might struggle with 6 layers.

    Crosstalk could also be an issue.

     

    Are you still doing anything related - just for fun?

    Feel free to contact me directly if more curious.

     

    No. I'm much happier not having to think about circuit design

    nowadays.  Wandering around europe is far nicer image

    Thanks for the invite anyway.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/148665

     

    --

    Best Regards:

                          Baron.