EAGLE User Support (English) Ground plane within a ground plane?
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
  • State Not Answered
  • Replies 6 replies
  • Subscribers 182 subscribers
  • Views 1215 views
  • Users 0 members are here
Related

Ground plane within a ground plane?

rickford66
rickford66 over 10 years ago

Hello all.  I'm currently using Eagle 6.5.0.  I want to put a ground all over my board on one of the inner layers.  It will cover my entire board with the exception of one small area.  In this area, I want to put another ground that is isolated from the larger ground all around it.  They must be on the same layer.  I tried drawing another polygon, expecting the existing all-over ground to give clearance, but that's not what happened.  No clearance was given.  I then drew around the area with a line and clearance was given for that.  That doesn't seem like a very clean way to do this.  What is the proper way to handle this?

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 10 years ago in reply to clem57 +1
    Clem Martins wrote: Why separate gnd planes? Curious George. The usual reason is to have separate analog and digital ground planes so that noisy digital signals don't couple to your analog circuits…
  • rickford66
    rickford66 over 10 years ago +1
    The reason for more than one ground plane is that one of the circuits is electrically isolated from the others. They're coupled together with opto-isolators. I had already tried giving it a different name…
  • clem57
    0 clem57 over 10 years ago

    Why separate gnd planes? Curious George.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 10 years ago in reply to clem57

    Clem Martins wrote:

     

    Why separate gnd planes? Curious George.

    The usual reason is to have separate analog and digital ground planes so that noisy digital signals don't couple to your analog circuits.  You also sometimes do this with an oscillator for similar reasons.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago

    If the plane is a polygon, then you can create another plane as a polygon too, and give them different 'rank' values (in the properties dialog). They will have clearance as long as they are different signals.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to shabaz

    On 18/04/15 02:29, shabaz wrote:

    If the plane is a polygon, then you can create another plane as a

    polygon too, and give them different 'rank' values

     

    The inner one being a numerically LOWER rank than the outer one.

     

    (in the properties

    dialog).

     

    Or in the drop-down on creation, or with "CHANGE RANK"...

     

    They will have clearance as long as they are different signals.

     

    ... which means you can't call them both "GND". You need to

    differentiate them on the schematic as different nets, say DGND and

    AGND. Then you need to connect them at only one point, using either a 0R

    link or, better, with one of the "short" components from (Olin's?)

    library for the purpose.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rickford66
    0 rickford66 over 10 years ago

    The reason for more than one ground plane is that one of the circuits is electrically isolated from the others.  They're coupled together with opto-isolators.

     

    I had already tried giving it a different name, as I would need to to get all the nets of that name to connect to it.  Giving it a higher rank than the surrounding plane did the trick.  There is now a small gap between the isolated ground and the rest of the ground.  Thanks.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to rickford66

    Thanks for that. I am learning as well as helping others learn. Wink winkimage

    Clem