EAGLE User Support (English) Ground plane within a ground plane?
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
  • State Not Answered
  • Replies 6 replies
  • Subscribers 182 subscribers
  • Views 1212 views
  • Users 0 members are here
Related

Ground plane within a ground plane?

rickford66
rickford66 over 10 years ago

Hello all.  I'm currently using Eagle 6.5.0.  I want to put a ground all over my board on one of the inner layers.  It will cover my entire board with the exception of one small area.  In this area, I want to put another ground that is isolated from the larger ground all around it.  They must be on the same layer.  I tried drawing another polygon, expecting the existing all-over ground to give clearance, but that's not what happened.  No clearance was given.  I then drew around the area with a line and clearance was given for that.  That doesn't seem like a very clean way to do this.  What is the proper way to handle this?

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 10 years ago in reply to clem57 +1
    Clem Martins wrote: Why separate gnd planes? Curious George. The usual reason is to have separate analog and digital ground planes so that noisy digital signals don't couple to your analog circuits…
  • rickford66
    rickford66 over 10 years ago +1
    The reason for more than one ground plane is that one of the circuits is electrically isolated from the others. They're coupled together with opto-isolators. I had already tried giving it a different name…
Parents
  • rickford66
    0 rickford66 over 10 years ago

    The reason for more than one ground plane is that one of the circuits is electrically isolated from the others.  They're coupled together with opto-isolators.

     

    I had already tried giving it a different name, as I would need to to get all the nets of that name to connect to it.  Giving it a higher rank than the surrounding plane did the trick.  There is now a small gap between the isolated ground and the rest of the ground.  Thanks.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rickford66
    0 rickford66 over 10 years ago

    The reason for more than one ground plane is that one of the circuits is electrically isolated from the others.  They're coupled together with opto-isolators.

     

    I had already tried giving it a different name, as I would need to to get all the nets of that name to connect to it.  Giving it a higher rank than the surrounding plane did the trick.  There is now a small gap between the isolated ground and the rest of the ground.  Thanks.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 10 years ago in reply to rickford66

    Thanks for that. I am learning as well as helping others learn. Wink winkimage

    Clem