EAGLE User Support (English) Design of PCBs
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
  • State Not Answered
  • Replies 5 replies
  • Subscribers 179 subscribers
  • Views 507 views
  • Users 0 members are here
  • frontpage
Related

Design of PCBs

Former Member
Former Member over 10 years ago

How to create exposed pads in Eagle packages??

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 10 years ago

    Hi Ashna,

     

    Put a polygon or rectangle on the tStop/bStop layer over the specific area on the top/bottom copper respectively. You don't usually need to do that, because pads already have that done for you. EAGLE is flexible and allows you to manually do it for certain use-cases.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to shabaz

    But then how do I name the polygon as the pin on the symbol of the device? There is no Name option which means that it won't be shown as connected. How do I fix that?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago in reply to shabaz

    But then how do I name the polygon as the pin on the symbol of the device? There is no Name option which means that it won't be shown as connected. How do I fix that?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 10 years ago in reply to Former Member

    Am 20.04.2015 um 13:39 schrieb Ashna Gupta:

    But then how do I name the polygon as the pin on the symbol of the

    device? There is no Name option which means that it won't be shown as

    connected. How do I fix that?

     

    Please read ...\doc\manual_en.pdf

     

    Chapter  8.14 Arbitrary Pad Shapes

     

     

    Mit freundlichen Grüßen / Best regards

     

    Alfred Zaffran

    --

    ______________________________________________________________

    Alfred Zaffran              Support

    CadSoft Computer GmbH       Hotline:   08635-698930

    Pleidolfweg 15              FAX:       08635-698940

    84568 Pleiskirchen          eMail: <alf@cadsoft.de>

                                 Web:   <www.cadsoft.de>

    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschaeftsfuehrer: Mark Whiteling

    ______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to Former Member

    Hi Ashna,

     

    Your question was "How to create exposed pads in Eagle packages??"

    and  the answer is (as mentioned) "You don't usually need to do that, because pads [i.e. through-hole pads, and smd] already have that done for you".

     

    Your further comment is a different question, but there is no context/explanation of what you're really trying to do, and this thread could end up very long if I just try to guess, so it will be better if you explain the scenario/use-case and then the requirement in detail.