EAGLE User Support (English) PCB component name (hierarchical design)
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
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 180 subscribers
  • Views 1279 views
  • Users 0 members are here
  • eagle
  • pcb
Related

PCB component name (hierarchical design)

apica
apica over 10 years ago

Hello,

I'm making a design with Eagle 7.2.0 and using the hierarchy feature. In each hierarchic bloc, the name of each component starts from 1 (U1, U2, ...). The problem is on the PCB design, because the hierarchic bloc name is added in each component.


For example, the bloc "SUPPLY" have the components C2 and R3. In the PCB view, the name of the components are the following:

image

Is it possible to show only the component identifier (C2 or R3) without showing the hierarchic bloc name (SUPPLY) on the PCB?

 

Thank you!

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 10 years ago in reply to Former Member +1
    On 22/12/15 16:32, sunny duan wrote: Professional PCB manufacturer here Really? Because as far as your presence here would indicate, you're actually a highly unprofessional SPAMMER. Go away.
  • clem57
    clem57 over 9 years ago in reply to autodeskguest +1
    Reported to moderator ty
Parents
  • clem57
    0 clem57 over 10 years ago

    No, this is not how it works. What you really do is compose a small schematic and expose the various leads. Please watch this demo to see how it works: https://www.youtube.com/watch?v=X7FkzqIGsqU

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago

    No, this is not how it works. What you really do is compose a small schematic and expose the various leads. Please watch this demo to see how it works: https://www.youtube.com/watch?v=X7FkzqIGsqU

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • apica
    0 apica over 10 years ago in reply to clem57

    Thank you for replying.

     

    I already saw this tutorial, and I made the supply module with the input/output leads.

    image

    And inside the module...

    image

     

    I'm just asking about the naming of the components in the board editor.

     

    Thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to apica

    In the tutorial they said the names inside were unique to outside. This implies they need to use a qualified name outside, hence the Supply:R3 for instance.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • apica
    0 apica over 10 years ago in reply to clem57

    Thank you, I only wanted to know if there is a way to change this.