Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 7.2 Win install directory -- why non-standard?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 24 replies
  • Subscribers 191 subscribers
  • Views 5481 views
  • Users 0 members are here
  • eagle
  • installation
Related

Eagle 7.2 Win install directory -- why non-standard?

gwideman
gwideman over 11 years ago

Hi all,

 

I went to install Eagle 7.2, and immediately got stuck when it offers a default install directory of C:\EAGLE-7.2.0.  OK, why?

 

In general I don't want apps installing themselves in random top-level locations; why can't Eagle just install in one of the standard locations?

 

So, I could just edit the suggested location, but to which standard location? Is Eagle a 32-bit app or a 64-bit app? And maybe there's some crucial reason why it can't be installed to one of those?

 

Eventually I found online a file "v7.2_en.pdf" EAGLE Update Information, which contains the enigmatic remark "On Windows the default installation path in the setup dialog has been changed from the Windows program folder to C:\EAGLE-<version> (<version> being the full EAGLE version string)." 

 

No explanation of why this change, and how crucial it is to abide by it. Maybe it's just a mistake?

 

FWIW, I changed the path to C:\Program Files (x86)\EAGLE-7.2.0. Even doing that was a hassle because the Browse window won't allow you to browse then enter the name of the new installation directory. But it is possible to back out of that window and enter the desired path by hand.

 

After installation, I checked the eagle.exe executable, and it is a 32-bit app, so I guessed correctly on the location.

 

Still don't know if this will cause problems downstream though.

 

Any further info on this?

 

-- Graham

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    Am 29.04.2015 um 06:21 schrieb Graham Wideman:

    Hi all,

     

    I went to install Eagle 7.2, and immediately got stuck when it offers a

    default install directory of C:\EAGLE-7.2.0.  OK, why?

     

    In general I don't want apps installing themselves in random top-level

    locations; why can't Eagle just install in one of the standard

    locations?

     

    So, I could just edit the suggested location, but to which standard

    location? Is Eagle a 32-bit app or a 64-bit app? And maybe there's some

    crucial reason why it can't be installed to one of those?

     

    Eventually I found online a file "v7.2_en.pdf" EAGLE Update Information,

    which contains the enigmatic remark "On Windows the default installation

    path in the setup dialog has been changed from the Windows program

    folder to C:\EAGLE-<version> (<version> being the full EAGLE version

    string)."

     

    No explanation of why this change, and how crucial it is to abide by it.

    Maybe it's just a mistake?

     

    FWIW, I changed the path to C:\Program Files (x86)\EAGLE-7.2.0. Even

    doing that was a hassle because the Browse window won't allow you to

    browse then enter the name of the new installation directory. But it is

    possible to back out of that window and enter the desired path by hand.

     

    After installation, I checked the eagle.exe executable, and it is a

    32-bit app, so I guessed correctly on the location.

     

    Still don't know if this will cause problems downstream though.

     

    Any further info on this?

     

    -- Graham

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/148455

     

     

    I think for making an installation easy, there must a path be given.

    But how should eagle know how many hard disks you have and how they are

    named?

    Then think of the structure of windows. There is the admin account and

    the users account which are different protected by the way.

    As a user the program  will be  ready under "username" and that's one

    reason why some people do not find their files image

    Install your program on any drive i.e. F:\eagle-xy  and not under

    c:\users, adjust the path in the control panel options and you are done image

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago

    Am 29.04.2015 um 06:21 schrieb Graham Wideman:

    Hi all,

     

    I went to install Eagle 7.2, and immediately got stuck when it offers a

    default install directory of C:\EAGLE-7.2.0.  OK, why?

     

    In general I don't want apps installing themselves in random top-level

    locations; why can't Eagle just install in one of the standard

    locations?

     

    So, I could just edit the suggested location, but to which standard

    location? Is Eagle a 32-bit app or a 64-bit app? And maybe there's some

    crucial reason why it can't be installed to one of those?

     

    Eventually I found online a file "v7.2_en.pdf" EAGLE Update Information,

    which contains the enigmatic remark "On Windows the default installation

    path in the setup dialog has been changed from the Windows program

    folder to C:\EAGLE-<version> (<version> being the full EAGLE version

    string)."

     

    No explanation of why this change, and how crucial it is to abide by it.

    Maybe it's just a mistake?

     

    FWIW, I changed the path to C:\Program Files (x86)\EAGLE-7.2.0. Even

    doing that was a hassle because the Browse window won't allow you to

    browse then enter the name of the new installation directory. But it is

    possible to back out of that window and enter the desired path by hand.

     

    After installation, I checked the eagle.exe executable, and it is a

    32-bit app, so I guessed correctly on the location.

     

    Still don't know if this will cause problems downstream though.

     

    Any further info on this?

     

    -- Graham

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/148455

     

     

    I think for making an installation easy, there must a path be given.

    But how should eagle know how many hard disks you have and how they are

    named?

    Then think of the structure of windows. There is the admin account and

    the users account which are different protected by the way.

    As a user the program  will be  ready under "username" and that's one

    reason why some people do not find their files image

    Install your program on any drive i.e. F:\eagle-xy  and not under

    c:\users, adjust the path in the control panel options and you are done image

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • gwideman
    0 gwideman over 11 years ago in reply to autodeskguest

    Joern: Thanks for replying, but your comment does not reconcile with how programs are customarily installed on Windows. There has historically been a \Program Files directory, and in 64-bit Windows there's also a \Program Files(x86) directory. These are usually on the first hard drive, which is usually called "C:". But installers don't have to know any of that, because they can use a shell variable %programfiles% or %programfiles(x86)%, which deals with the possibility of a non-standard file layout. Applications are almost never installed to a user's home directory (though a script might be).

     

    So if there's a reason for Eagle offering/suggesting to install in its own top-level directory, it's not because it's too difficult for the installer to figure out the conventional place to install.

     

    -- Graham