Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 7.2 Win install directory -- why non-standard?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 24 replies
  • Subscribers 191 subscribers
  • Views 5442 views
  • Users 0 members are here
  • eagle
  • installation
Related

Eagle 7.2 Win install directory -- why non-standard?

gwideman
gwideman over 11 years ago

Hi all,

 

I went to install Eagle 7.2, and immediately got stuck when it offers a default install directory of C:\EAGLE-7.2.0.  OK, why?

 

In general I don't want apps installing themselves in random top-level locations; why can't Eagle just install in one of the standard locations?

 

So, I could just edit the suggested location, but to which standard location? Is Eagle a 32-bit app or a 64-bit app? And maybe there's some crucial reason why it can't be installed to one of those?

 

Eventually I found online a file "v7.2_en.pdf" EAGLE Update Information, which contains the enigmatic remark "On Windows the default installation path in the setup dialog has been changed from the Windows program folder to C:\EAGLE-<version> (<version> being the full EAGLE version string)." 

 

No explanation of why this change, and how crucial it is to abide by it. Maybe it's just a mistake?

 

FWIW, I changed the path to C:\Program Files (x86)\EAGLE-7.2.0. Even doing that was a hassle because the Browse window won't allow you to browse then enter the name of the new installation directory. But it is possible to back out of that window and enter the desired path by hand.

 

After installation, I checked the eagle.exe executable, and it is a 32-bit app, so I guessed correctly on the location.

 

Still don't know if this will cause problems downstream though.

 

Any further info on this?

 

-- Graham

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    Hi Graham,

     

    The reason we changed the default installation path is to avoid the

    virtualisation issues in newer Windows (it started in Vista and then

    took hold from there).

     

    Many users don't bother to check where they save their work and often

    save into EAGLE's installation directory. With the UAC features the

    write get redirected without the user ever knowing.

     

    When they try to find the files through Windows explorer they don't

    appear and panic ensues. This behaviour caused us (the support staff

    specifically) a lot of head aches and calls. So the decision was made to

    simply change the default path to avoid the issue altogether.

     

    One could argue that the correct solution would be to conform to Windows

    file conventions and make any necessary adjustment to where our

    libraries and such are stored to avoid this issue. At this time we want

    to minimize any special considerations based on OS so that is the

    decision we went with.

     

    Computer savy users can usually figure out what's going and save their

    work elsewhere, but unfortunately they don't make up the majority of

    EAGLE users.

     

    Basically, as long as you don't save any of your work into the

    installation directories, or try to modify anything in the installation

    directories then you won't have problems.

     

    I hope this gives you some insight.

     

    Best Regards,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gwideman
    0 gwideman over 11 years ago in reply to autodeskguest

    Jorge and all:

     

    First off, thanks for filling me in on the rationale for why the change of install directory. That allows me to assess the alternatives. Here's what I think I learned.

     

    Apparently the problem to be solved was that users were saving their docs to the default location offered by Eagle's Save dialog, which was set to point to a directory within the Eagle application directory. That has not been a reasonable location to store user docs at least as far back as WinXP, so over 13 years.

     

    Windows has increasingly attempted to protect application directories against arbitrary writes by nonprivileged users. So in recent versions of Windows, attempts by applications (perhaps running with non-admin permissions) to save user files to their app directories have been redirected to the specific user's VirtualStore:

     

    So, the app tries to save to C:\Program Files (x86)\EAGLE-6.5.0

     

    Windows saves that to:

     

    C:\Users\[user]\AppData\Local\VirtualStore\Program Files (x86)\EAGLE-6.5.0.

     

    (I'm assuming that Eagle 6.5's Open dialog would see into the VirtualStore when opening -- that is Save and Open were symmetrical, though I have not tried it myself.)

     

    Amongst other things, it means multiple users using the same copy of Eagle don't overwrite each other's files.

     

    However, if users use Windows Explorer to go looking for their files where they think they put them, obviously they will be surprised.

     

    Let's be clear, however, that this is not intended to be a good way of doing things. It is simply a way for Windows to tighten security while dealing with legacy applications that don't properly deal with saving files.

     

    There is nothing to stop Eagle from making sure that the Save dialog defaults to some directory other than the application directory. A decent choice would be within the User's home directory:

     

    C:\Users\[user]\Documents\Eagle

     

    or similar. And there are OS variables that an app can use to easily determine that directory, even if the user has located it somewhere else.

     

    Of course, a slightly more savvy user might use Eagle settings to specify a different directory, as is current practice, especially for multiple users sharing files, perhaps on a server.

     

    The point is, on no platform should Eagle be storing user documents in the application's installation directory. Surely it doesn't do so on Mac or linux? So why would it suggest to do so on Windows?

     

    Bottom line: from what I've heard so far, it seems to me that the change to a non-standard installation directory was primarily a coarse fix for the fine-scale issue of simply pointing the Save and Open dialogs to a sensible default location.

     

    -- Graham

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to gwideman

    On 29.04.2015 23:10, Graham Wideman wrote:

    Jorge and all:

     

    Bottom line: from what I've heard so far, it seems to me that the change

    to a non-standard installation directory was primarily a coarse fix for

    the fine-scale issue of simply pointing the Save and Open dialogs to a

    sensible default location.

     

    You seen to know what you're talking about. Maybe you could explain what

    Cadsoft (or users, by manually choosing non program folder) risk by

    simply putting an executable onto a common folder?

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gpsmikey
    0 gpsmikey over 11 years ago in reply to autodeskguest

    Very good information.  I guess from my knothole (and many others), the

    biggest problem with the "virtualization" scheme that M$ implemented is the

    fact that they don't bother to tell you they didn't put your files where

    you thought you put them.  Give me a pop-up indicating the specified

    location is NOT legal for user files and where they are being stored.  Most

    people that run into this don't have a clue what happened.  And it can be

    pretty insidious at times - different software, the company sent me a new

    key file by email.  I grabbed the keyfile (license) and dragged it onto the

    install directory for their software (where it belonged).  Didn't work -

    seems if you drag from the email, it does not have the rights to be put in

    the install directory (under /Program Files(x86) ) so it puts it in the

    virtual store WITHOUT telling you.  If you drag it to the desktop first

    THEN to the install directory, that works (at least as an admin).  I

    understand the attempt to protect the install directories, but TELL the

    user you did not do what they asked, not simply do something else then say

    "OK".

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to gwideman

    Hi Graham,

     

    I actually have an element-14 account, the problem is that I access the

    newsgroups through Thunderbird and NNTP. Element14's interface to this

    server is less than stellar and this is just one of it's issues.

     

    I don't want to go through the web portal so I just deal with the

    Cadsoft guest situation by writing my name in every post I write. So if

    you see my name you know its me.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to gwideman

    Hi Graham,

     

    I actually have an element-14 account, the problem is that I access the

    newsgroups through Thunderbird and NNTP. Element14's interface to this

    server is less than stellar and this is just one of it's issues.

     

    I don't want to go through the web portal so I just deal with the

    Cadsoft guest situation by writing my name in every post I write. So if

    you see my name you know its me.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • gpsmikey
    0 gpsmikey over 11 years ago in reply to autodeskguest

    Very good information.  I guess from my knothole (and many others), the

    biggest problem with the "virtualization" scheme that M$ implemented is the

    fact that they don't bother to tell you they didn't put your files where

    you thought you put them.  Give me a pop-up indicating the specified

    location is NOT legal for user files and where they are being stored.  Most

    people that run into this don't have a clue what happened.  And it can be

    pretty insidious at times - different software, the company sent me a new

    key file by email.  I grabbed the keyfile (license) and dragged it onto the

    install directory for their software (where it belonged).  Didn't work -

    seems if you drag from the email, it does not have the rights to be put in

    the install directory (under /Program Files(x86) ) so it puts it in the

    virtual store WITHOUT telling you.  If you drag it to the desktop first

    THEN to the install directory, that works (at least as an admin).  I

    understand the attempt to protect the install directories, but TELL the

    user you did not do what they asked, not simply do something else then say

    "OK".

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.