EAGLE User Support (English) New to PCB design and really need a hand.
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
  • State Not Answered
  • Replies 10 replies
  • Subscribers 179 subscribers
  • Views 732 views
  • Users 0 members are here
Related

New to PCB design and really need a hand.

Former Member
Former Member over 10 years ago

Hi there, I am trying to make some simple PCBs to use as a test fixture for some ribbon cables I work with. The board layout is very simple, but I cannot seem to figure out the correct way to actually lay it out. I have a 2D CAD drawing that I did in AutoSketch which I will attach. So far I have tried EagleCAD, DipTrace, ExpressPCB, PCB123, and PCB Web Designer, and the only program I have managed to successfully design the board in is (unfortunately) PCB123, but their prices are outrageous, and I cannot export gerber files. I will attach the PCB123 files as well.

 

I really want to learn how to use EagleCAD properly, but at the same time I am on a huge crunch to get these boards done as soon as possible. Does anyone have any good recommendations? or would anyone we willing to take my current drawings into eagle and help me out?  

 

Any help is greatly appreciated.

 

Parts:

-The top 2 connectors are 13pos pin headers, the same size you'd find on a PC motherboard, Arduino, or RaspberryPi. (The part numbers in my first drawing may actually be wrong)

 

-The Bottom 2 are the special Molex connectors that the cables use. there is a 12 and 13 pos connector. they can be found on DigiKey (links below)

12 pos http://www.digikey.com/product-search/en?x=0&y=0&lang=en&site=us&keywords=WM1741-ND

13 pos 53047-1310 Molex Connector Corporation | WM17003-ND | DigiKey

Attachments:
image
test fixture PCB123.zip
  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 10 years ago

    Here is a quick tutorial I made that includes step by step instructions on how to create a PCB and manufacturing artwork:

    Eagle Design demo

    There are other tutorials on the web that may also help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to dougw

    On 2/05/2015 5:34 p.m., Douglas Wong wrote:

    Here is a quick tutorial I made that includes step by step instructions

    on how to create a PCB and manufacturing artwork:

     

    There are other tutorials on the web that may also help.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/148689

     

     

    Pity you have instructional errors in the tutorial.

     

    You should not use the WIRE tool to connect schematic parts. That is bad

    practice and to many issues arise by doing so. You use the NET tool.

    You will also not need to use the JUNCTION tool if you follow the

    practice of using the NET tool as junctions will be set automatically if

    you start or end on a net.

     

     

    HTH

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to autodeskguest

    On 02/05/15 08:08, warrenbrayshaw wrote:

     

    Pity you have instructional errors in the tutorial.

     

     

    Eagle isn't the only tool affected by the Internet phenomenon of

    "tutorials" written (or video'd) by people who apparently haven't taken

    the trouble to go through the manufacturer's tutorial that comes with

    the product image

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to autodeskguest

    On 02/05/15 08:08, warrenbrayshaw wrote:

     

    Pity you have instructional errors in the tutorial.

     

     

    Eagle isn't the only tool affected by the Internet phenomenon of

    "tutorials" written (or video'd) by people who apparently haven't taken

    the trouble to go through the manufacturer's tutorial that comes with

    the product image

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • COMPACT
    0 COMPACT over 10 years ago in reply to autodeskguest

    Warren,

    image Are you sure it's not just a matter of a different method rather than an "Error"?

    I have just looked at the manufacturer's manual (V7.2 3rd edition) and it says you can use either the WIRE (page 59) or NET (page 61) tool for electrical connections.

    Page 73 also says that if WIRES are used for layers 1-16 they are electrical connections.

    The walkthrough (on page 121) just happens to use the NET tool and it goes on to say that JUNCTIONs are not necessarily automatically placed but a user configurable option.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to COMPACT

    On 3/05/2015 6:21 p.m., COMPACT wrote:

    Warren,

    image Are you sure it's not just a matter of a different method rather than

    an "Error"?

    I have just looked at the manufacturer's manual (V7.2 3rd edition) and

    it says you can use either the WIRE (page 59) or NET (page 61) tool for

    electrical connections.

    Page 73 also says that if WIRES are used for layers 1-16 they are

    electrical connections.

    The walkthrough (on page 121) just happens to use the NET tool and it

    goes on to say that JUNCTIONs are not necessarily automatically placed

    but a user configurable option.

     

    Hi

    When you quote the manual, please first understand the context.i.e Which

    editor is being talked about.

     

    Page 59 says "Draw line (this command is called WIRE because it is used

    to define

    electrical connections, i.e. wires, in the Layout Editor)." The Layout

    editor is the board editor, not the schematic editor.

     

    Page 73 is talking of the board or package editors. That is where you

    find layers 1-16.

     

    The Manual Page 121 says "Nets must be drawn with the NET command, not

    with the WIRE command." and there is good reason.

     

    Novices have some initial success using the wire tool but then they

    appear on the forum asking why things aren't working so well for them.

    There are some things that work better with the net tool rather than a

    wire on the net layer.

     

    The behaviour is different.

    (1) The net command terminates when reaching a pin. The wire does not.

    (2) The junction dot can occur automatically with nets but not with

    wires on layer 91.

    (3) Draw a wire on a layer that is not the net layer and you need to

    switch to the wire layer manually when you wish to draw a net. Using the

    net tool, the net layer is automatically selected.

    (4) Try using a wire to pull a net name out of a Bus. You cannot do it

    with Wire but Net permits it.

     

    There are no doubt other reasons but the one I like the best is that net

    represents a logical connection. As schematics become more complex you

    do not wire between points you simply show the logical connection with

    the net. Its a good practice to get into.

     

    So, if you wish, you can use the wire tool for nets in most instances

    but you loose some of the automation that has been given to the net tool.

     

    HTH

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • COMPACT
    0 COMPACT over 10 years ago in reply to autodeskguest

    Thanks Warren,

    This issue must keep you quite busy.

     

    image My confusion is caused by the Schematic Editor's "Draw Line" tool being called and annotated as "WIRE" and defaulting to place a "NET".

    (Plus the mentioning of electrical connections within the WIRE / Draw Line for the Schematic Editor).

     

    Is there going to be anything done to remedy this confusion by a manual or software alteration?

     

    Very Compact

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to COMPACT

    On 5/3/2015 6:52 AM, COMPACT wrote:

    Thanks Warren,

    This issue must keep you quite busy.

     

    image My confusion is caused by the Schematic Editor's "Draw Line" tool

    being called and annotated as "WIRE" and defaulting to place a "NET".

    (Plus the mentioning of electrical connections within the WIRE / Draw

    Line for the Schematic Editor).

     

    Is there going to be anything done to remedy this confusion by a manual

    or software alteration?

     

    Hi Compact,

     

    I've been fighting to get that thing renamed to LINE or something else

    to alleviate the confusion. I've been seeing a glimmer of hope lately so

    we'll see.

     

    Like Warren said, stick to the NET tool if you do that everything will

    work as expected.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • COMPACT
    0 COMPACT over 10 years ago in reply to autodeskguest

    Hi Jorge,

    From the behaviour observed from the EAGLE program and the information provided by Warren and yourself it appears that NET tool is derived from the WIRE tool with extra (or alternate) code attached to handle electrical net connections such as connections to busses and other nets.

    Is this correct?

     

    If so, is it possible as an added feature to EAGLE to adjust the behaviour of the NET tool so that when an existing net is connected to a BUS and when the net is not a member of the BUS to pop up a dialog box with the option to add the existing net to the BUS rather than just popping up an error message?

    e.g. "Net D7 is not a member of D[0..6]. Add D7 as a member to the BUS?"

     

    And/or add some logic to WIRE in the schematic editor to behave as NET tool if layer 91 is selected.

     

    If both tools must be present is it also possible to change the NET's icon and position within the Schematic Editor toolbar so it appears before the WIRE/Draw Line tool be default?

    This should prevent noobs from using the WIRE/Draw Line tool for placing NETs.

     

    Best Regards

     

    Very Compact

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • COMPACT
    0 COMPACT over 10 years ago in reply to COMPACT

    And also adjusting the BUS tool so that if a new one is placed over the ends of existing nets that it gives you the option to add those nets to the newly placed BUS?

     

    This'll be very handy and speed up schematic capture.