EAGLE User Support (English) Straition lines printing in filled areas
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
  • State Not Answered
  • Replies 22 replies
  • Subscribers 183 subscribers
  • Views 3577 views
  • Users 0 members are here
  • lines
  • fill
Related

Straition lines printing in filled areas

Former Member
Former Member over 10 years ago

OS= Win 8.1

Eagle = 7.2

 

I have a direct to board print setup. That is, I print directly on the copper clad, straight out of Eagle. I have noticed that the fill lines are showing. I have found where others have had this issue, but I have not understood what to do to resolve the problem. This problem also occurs when I print the PCB to pdf format. I have read that it has to do with Eagle using lines to cover the filled area and that changing the line width and the fill style might be helpful. But, then, there are no instructions on how to do these operations and no feedback as to whether it worked, or not. Would someone please be so kind as to tell me the definitive cure and the steps to complete the task? I would be very grateful. Eagle files and libraries are attached. The problem is very clear in the pdf format. Thank you very much for your help.

Attachments:
Oscilloscope.zip
  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago +1
    Maybe you need to do a Polygon command setting the color. See PCB Creation with Eagle for Beginners : The Ground Plane There is more about polygon HOW-TO: Polygons and ground fills for PCBs in Eagle |…
  • balearicdynamics
    balearicdynamics over 10 years ago +1
    t1d I have downloaded the attached zip file and opened it on eagle checking for the schematics you included in PDF. The point is that the pdf is different than the schematics you attached, as in the image…
  • Bertl
    Bertl over 10 years ago in reply to balearicdynamics +1
    If you press the button "Ratsnest" (first one in the last button section, the one with the connected nodes), you will see that the area enclosed by the dashed line will fill up (flood) the free space around…
Parents
  • clem57
    0 clem57 over 10 years ago

    Maybe you need to do a Polygon command setting the color. See PCB Creation with Eagle for Beginners : The Ground Plane

    There is more about polygon HOW-TO: Polygons and ground fills for PCBs in Eagle | Dangerous Prototypes

     

    clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago

    Maybe you need to do a Polygon command setting the color. See PCB Creation with Eagle for Beginners : The Ground Plane

    There is more about polygon HOW-TO: Polygons and ground fills for PCBs in Eagle | Dangerous Prototypes

     

    clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    Hi, Clem, Thank you for trying to help me.

     

    I believe that I am creating the polygons correctly. The color of the fill is determined by the color of the layer on which the polygon is placed.

     

    The different layer colors are for visualization purposes. To print, I check the black box and everything prints in black. However, the polygons, which are supposed to be filled solid, have striations in them.

     

    Striations are lines of thicker (more ink) and thinner (less ink) ink coverage. The thinner ink lines are prone to cause etching failures.

     

    Eagle uses lines to fill polygons. That is to say that the fill of the polygon, which appears to be solid, is actually created with stacks of lines. When the lines are overlapping properly, the polygon appears, to the eye, to be solid. The fill lines in my polygons are not overlapping properly. So, I need to discover how to fix the overlap.

     

    Thanks for your interest!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to Former Member

    Is this an issue? http://www.element14.com/community/thread/17442/l/why-does-eagle-print-everything-thicker

    But if you are using a PDF see this http://indesignsecrets.com/when-you-see-thin-white-lines-in-your-pdf-files.php

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    Thank you, Clem, for your continued support. Of the two links you provided:

    1) The first identifies a problem of spreading ink, due to using the heat transfer method, when the traces, and their clearances, are very small.

    2) The second identifies a problem of striations in the fill, but it only occurs in exported pdf files. The solution was outside of Eagle and with a different method, TBICT. They also increased the dpi, which I have done, prior; I'm using 1200 dpi and still getting the problem. It also happens, regardless of what printer that I am using.