EAGLE User Support (English) Straition lines printing in filled areas
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
  • State Not Answered
  • Replies 22 replies
  • Subscribers 183 subscribers
  • Views 3570 views
  • Users 0 members are here
  • lines
  • fill
Related

Straition lines printing in filled areas

Former Member
Former Member over 10 years ago

OS= Win 8.1

Eagle = 7.2

 

I have a direct to board print setup. That is, I print directly on the copper clad, straight out of Eagle. I have noticed that the fill lines are showing. I have found where others have had this issue, but I have not understood what to do to resolve the problem. This problem also occurs when I print the PCB to pdf format. I have read that it has to do with Eagle using lines to cover the filled area and that changing the line width and the fill style might be helpful. But, then, there are no instructions on how to do these operations and no feedback as to whether it worked, or not. Would someone please be so kind as to tell me the definitive cure and the steps to complete the task? I would be very grateful. Eagle files and libraries are attached. The problem is very clear in the pdf format. Thank you very much for your help.

Attachments:
Oscilloscope.zip
  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago +1
    Maybe you need to do a Polygon command setting the color. See PCB Creation with Eagle for Beginners : The Ground Plane There is more about polygon HOW-TO: Polygons and ground fills for PCBs in Eagle |…
  • balearicdynamics
    balearicdynamics over 10 years ago +1
    t1d I have downloaded the attached zip file and opened it on eagle checking for the schematics you included in PDF. The point is that the pdf is different than the schematics you attached, as in the image…
  • Bertl
    Bertl over 10 years ago in reply to balearicdynamics +1
    If you press the button "Ratsnest" (first one in the last button section, the one with the connected nodes), you will see that the area enclosed by the dashed line will fill up (flood) the free space around…
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    On 29.05.2015 02:53, Tee Dunn wrote:

    Did you have this problem, yourself, and, then, learned that using the

    "solid" function was the cure. Or, do you just know that the "solid"

    function exists? I mean that as a genuine question... I don't mean to be

    brash... It just would help me to know where you are coming from.

     

    I explained earlier a bit where I bumped into a similar issue.

     

    To elaborate a bit, years ago, I was generating files for a high density

    board, and the board house came back to me with a similar issue as you

    describe. They didnt use pdf, but gerbers. Apparently their tool

    (unknown) converted wire fills to polygon fills, and it was not able to

    see this as a fill because of these lines.

     

    Changing the gerber format from GERBER_RS274X to GERBER_RS274X_25 fixed

    that problem back then, but I ended up writing my own gerber export ulp

    because they wanted all pads flashed, but that is a different story.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    On 29/05/2015 12:53 p.m., Tee Dunn wrote:

    In the print dialog, when you select 'black', you should also select

    'solid'. If you fail to do that and your layer setup does not have a

    solid fillstyle then you can get the light and dark stripes.

    ++

    HTH

    Warren

     

    I have tried that, too. It did not fix the problem for me.

     

    Did you have this problem, yourself, and, then, learned that using the

    "solid" function was the cure. Or, do you just know that the "solid"

    function exists? I mean that as a genuine question... I don't mean to be

    brash... It just would help me to know where you are coming from.

     

    I use solid fills for all planes. Eagle translates them as lines.

    Whether the solid function is on, or not, Eagle still renders solids as

    lines.

     

    You have good insights and I appreciate your help.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/151006

     

    Time for some clarity

    v7.2.2

    When I display your pdf I do not see lines

    When I print your pdf I do not see lines.

    When I open your board and print to pdf I do not get lines when I

    display the pdf or when I print it.

     

    So you have an issue I do not have, so something in your environment is

    creating the issue for you.

     

    Remember when you send a board file to someone, your layer settings do

    not go with it. I see the board with my palette settings.

     

    I then experimented to see what I had to do to get the type of lines you

    report.The only way was to change the fill of a layer colour and print

    without the Solid checkbox checked.

     

    You say your fill lines are not overlapping fully. Please show us how it

    looks on your computer with a screen shot of the polygon construction

     

    key the following into the command line

    SET FILL_LAYER 16 0; rats;

     

    You should be able to inspect for no overlap which I don't think you

    will see. If you do, take a screen shot of the failing area and post it

    back here in the thread.

     

    Then try

    SET FILL_LAYER 16 2; rats;

    Print to pdf, without 'solid' selected. I get striping but only on some

    of the magnifications but importantly does happen at 100%

     

    key the following to return it to solid fill for layer 16

    SET FILL_LAYER 16 1; rats;

     

    All the best

    Warren

     

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<